Available by clicking the More... button in the Computed Channel dialog box. This dialog box allows you to enter strain equation constants, which are typically supplied by the strain gage manufacturer.
Enter the Gage Factor. The default is 2.0
Enter the value of the unstrained bridge output voltage (Vout). The default value is 0.0 volts. After entering the strain equation constants, click OK to save the constants.