Available by clicking
when the monitor channel is displayed. This window allows you to select a monitor
channel on an instrument and set the monitor channel attributes. You can adjust the window's horizontal position by clicking on the window and dragging it left or right.
Note: If the monitor channel is not displayed, select "Show Monitor Channel" from the Application Settings
menu.
Select Channel - Use the drop-down list to select a channel to monitor on the selected instrument. Note that the list is automatically pre-populated with all channels included in the current scan list.
Note: Channels must be part of the scan list (Configure Channels tab) to be shown in the Select Channel drop-down list.
Select either Decimal or Hex format when monitoring a digital I/O channel on the 34907A Multi-Function Module or DAQM907A Multi-Function Module.
Change the displayed background and/or text color. To change a color, use the drop-down to select either Background or Text. Click the color palette drop-down list to select the desired background color or text color.