Cannot Access Remote Interface
Problem:
You cannot access devices on a remote GPIB, remote USB, or remote serial interface that was previously functional.
Probable Causes:
- The remote I/O server or gateway hosting the remote devices may be turned off or disabled.
- The configuration of the interface on the remote PC may have changed in a way that requires the Remote IO Server software on that PC to be restarted.
Suggested Steps:
- Ensure that the remote PC or gateway to which the devices are connected is turned on.
- Ensure that the Remote IO Server software is running on the remote PC or gateway.
- Stop the Remote IO Server software on the remote PC or gateway, then restart it.
More Information:
If the SICL interface ID or logical unit of a shared GPIB, USB, or serial interface is changed on a remote I/O server, that interface cannot be accessed remotely until the Remote IO Server software is stopped and restarted.