IAsyncMessage::SoftwareManufacturerID

Description

The ID number of the vendor of this software component.

VB Prototype

Dim value As Short
value = object.SoftwareManufacturerID

C++ Prototype

HRESULT get_SoftwareManufacturerID(
  short* SoftwareManufacturerID
);

Return Value

Refer to the table of return codes.

See Also

ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, IOProtocol, SendEndEnabled, TerminationCharacter, TerminationCharacterEnabled, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, AssertTrigger, Clear, ReadSTB, Read, Write, WriteString, Terminate, IAsyncMessage Overview