IEventTrigger::TriggerID
Description
The identifier of the triggering mechanism on which the specified trigger event was received.
VB Prototype
Dim value As
TriggerLine
value = object.TriggerID
C++ Prototype
HRESULT get_TriggerID(
TriggerLine* TriggerID
);
Return Value
Refer to the table of return codes.
See Also
type, CustomEventTypeNumber, TriggerID, GetAttribute, SetAttribute, Close, IEventTrigger Overview