IEventUsbInterrupt::InterruptSize
Description
Returns the actual number of bytes received.
VB Prototype
Dim value As Short
value = object.InterruptSize
C++ Prototype
HRESULT get_InterruptSize(
short* InterruptSize
);
Return Value
Refer to the table of return codes.
See Also
type, CustomEventTypeNumber, DataBuffer, Close, InterruptSize, IOStatus, IEventUsbInterrupt Overview