ITcpipSocket2::ServerCertificateIsPerpetual
Description
Returns a value indicating whether the server certificate is perpetual or not.
VB Prototype
Dim value As Boolean
                                            value = object.ServerCertificateIsPerpetual
                                        
C++ Prototype
HRESULT get_ServerCertificateIsPerpetual(
                                        
  VARIANT_BOOL* ServerCertificateIsPerpetual
);
Return Value
Refer to the table of return codes.
See Also
Address, Close, ComponentVersion, Flush,GetAttribute, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, HostName, Init, KeepAlive, LockRsrc, LastStatus, , LockState, NoDelay, OptionString, Port, , ProgID, ResourceName, ServerCertificate, ServerCertificateExpirationDate, ServerCertificateIsPerpetual, ServerCertificateIssuerName, ServerCertificateSubjectName, SessionType, SetAttribute, SetBufferSize, SoftwareManufacturerID, SoftwareManufacturerName, SpecVersion, Timeout, TlsCipherSuite , UnlockRsrc, ITcpipSocket2 Overview