Keysight VISA.NET Help
GlobalResourceManager Class Members
Properties  Methods 


The following tables list the members exposed by GlobalResourceManager.

Public Properties
 NameDescription
Public Propertystatic (Shared in Visual Basic)ImplementationVersion The version of this VISA.NET implementation.  
Public Propertystatic (Shared in Visual Basic)SpecificationVersion The version of the VISA.NET specification with which this VISA.NET implementation complies.  
Top
Public Methods
 NameDescription
Public Methodstatic (Shared in Visual Basic)FindOverloaded.  Find all of the VISA resources available on the system.  
Public Methodstatic (Shared in Visual Basic)OpenOverloaded.  Create a VISA I/O resource session.  
Public Methodstatic (Shared in Visual Basic)ParseParse the specified resourceName to get extended interface information.Parse the specified resourceName to get extended interface information.  
Public Methodstatic (Shared in Visual Basic)TryParseParse the specified resourceName to get extended interface information. If the Parse operation is not successful, this function returns false instead of throwing an exception.Parse the specified resourceName to get extended interface information. If the Parse operation is not successful, this function returns false instead of throwing an exception.  
Top
See Also

Reference

GlobalResourceManager Class
Ivi.Visa Namespace

 

 


© Keysight Technologies 2015-2025