Keysight VISA.NET Help
IMemoryMap Interface Properties

For a list of all members of this type, see IMemoryMap members.

Public Properties
 NameDescription
 PropertyAddressSpace The address space that is currently mapped to this session.  
 PropertyBaseAddressThe starting address of the memory AddressSpace that is currently mapped to this session.  
 PropertySizeThe size of the memory AddressSpace that is currently mapped to this session, starting at the BaseAddress  
 PropertyVirtualAddress Returns IntPtr.Zero if the window is only accessible through the operations provided on this interface. A return value other than IntPtr.Zero indicates you can dereference the mapped address as a pointer.  
Top
See Also

Reference

IMemoryMap Interface
Ivi.Visa Namespace

 

 


© Keysight Technologies 2015-2025