| Ivi.Visa Namespace > IMessageBasedFormattedIO Interface : PrintfAndFlush Method |
| Overload | Description |
|---|---|
| PrintfAndFlush(String) | Print a string to the formatted I/O write buffer, then send the buffer contents to the device with a newline character and flush the buffer. See Using Printf for detailed information. |
| PrintfAndFlush(String,Object[]) | Print formatted output to the formatted I/O write buffer, then send the buffer contents to the device with a newline character and flush the buffer. See Using Printf for detailed information. |
Current with Keysight IO Libraries Suite 18