Keysight VISA.NET Help
ReadBinaryBlockOfByte Method



See Using Read Methods for detailed information.
Overload List
OverloadDescription
ReadBinaryBlockOfByte() Read an array of bytes from the formatted I/O read buffer.  
ReadBinaryBlockOfByte(Boolean) Read an array of bytes from the formatted I/O read buffer.  
ReadBinaryBlockOfByte(Byte[],Int64,Int64)Read an array of bytes from the formatted I/O read buffer and store a maximum of count elements into data starting at index.  
ReadBinaryBlockOfByte(Byte[],Int64,Int64,Boolean)Read an array of bytes from the formatted I/O read buffer and store a maximum of count elements into data starting at index.  
Remarks

If BinaryEncoding = DefiniteLengthBlockData or BinaryEncoding = IndefiniteLengthBlockData: The ReadBinaryBlockOfByte method exhibits the same behavior as Scanf("%b", out result ), which returns result.

If BinaryEncoding = RawBigEndian: The ReadBinaryBlockOfByte method exhibits the same behavior as Scanf("%!oby", out result ), which returns result.

If BinaryEncoding = RawLittleEndian: The ReadBinaryBlockOfByte method exhibits the same behavior as Scanf("%!oly", out result ), which returns result.

 

Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025