Keysight VISA.NET Help
ReadLineBinaryBlockOfByte Method



See Using Read Methods for detailed information.
Overload List
OverloadDescription
ReadLineBinaryBlockOfByte() Read an array of bytes from the formatted I/O read buffer, then read and discard characters up to and including the next newline character.  
ReadLineBinaryBlockOfByte(Boolean) Read an array of bytes from the formatted I/O read buffer, then read and discard characters up to and including the next newline character.  
ReadLineBinaryBlockOfByte(Byte[],Int64)Read an array of bytes from the formatted I/O read buffer and store the elements into data starting at index. Then read and discard characters up to and including the next newline character.  
ReadLineBinaryBlockOfByte(Byte[],Int64,Boolean)Read an array of bytes from the formatted I/O read buffer and store the elements into data starting at index. Then read and discard characters up to and including the next newline character.  
Remarks

If BinaryEncoding = DefiniteLengthBlockData or BinaryEncoding = IndefiniteLengthBlockData: The ReadLineBinaryBlockOfByte method exhibits the same behavior as Scanf("b*T", out result ), which returns result.

If BinaryEncoding = RawBigEndian: The ReadLineBinaryBlockOfByte method exhibits the same behavior as Scanf("y*T", out result ), which returns result.

If BinaryEncoding = RawLittleEndian: The ReadLineBinaryBlockOfByte method exhibits the same behavior as Scanf("!oly*T ", out result ), which returns result.

Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025