Keysight VISA.NET Help
ReadLineListOfSByte() Method



Read a comma separated list of signed bytes from the formatted I/O read buffer and store them into the return array starting at index 0, then read and discard characters up to and including the next newline character.
Syntax
'Declaration
 
Overloads Function ReadLineListOfSByte() As SByte()
'Usage
 
Dim instance As IMessageBasedFormattedIO
Dim value() As SByte
 
value = instance.ReadLineListOfSByte()
sbyte[] ReadLineListOfSByte()
array<sbyte>^ ReadLineListOfSByte(); 

Return Value

An array of signed bytes.
Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025