Keysight VISA.NET Help
ReadListOfByte Method



See Using Read Methods for detailed information.
Overload List
OverloadDescription
ReadListOfByte(Int64)Read a comma separated list of bytes from the formatted I/O read buffer and store a maximum of count elements into the return array starting at index 0.  
ReadListOfByte(Byte[],Int64,Int64)Read a comma separated list of bytes from the formatted I/O read buffer and store a maximum of count elements into data starting at index.  
Remarks

The ReadListOfByte method exhibits the same behavior as Scanf("%,u", out result ), which returns result.

Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025