Keysight VISA.NET Help
TerminationCharacterEnabled Property (IMessageBasedSession)



If true, reads end when a termination character is received.
Syntax
'Declaration
 
Property TerminationCharacterEnabled As Boolean
'Usage
 
Dim instance As IMessageBasedSession
Dim value As Boolean
 
instance.TerminationCharacterEnabled = value
 
value = instance.TerminationCharacterEnabled
bool TerminationCharacterEnabled {get; set;}
property bool TerminationCharacterEnabled {
   bool get();
   void set (    bool value);
}
Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025