Keysight VISA.NET Help
INativeVisaEventArgs Interface Properties

For a list of all members of this type, see INativeVisaEventArgs members.

Public Properties
 NameDescription
 PropertyEventArgs An event args reference for the native C event. This may reference an object that derives from EventArgs, if the event handler for the event specified by the EventArg.EventType of EventArg.CustomEventType properties uses a derived class.  
Top
See Also

Reference

INativeVisaEventArgs Interface
Ivi.Visa Namespace

 

 


© Keysight Technologies 2015-2025