Keysight VISA.NET Help
GetAttributeString Method (INativeVisaEventArgs)



Retrieve the value of the specified attribute from the native C implementation.
Overload List
OverloadDescription
GetAttributeString(NativeVisaAttribute) Retrieve the value of the specified attribute from the native C implementation.  
GetAttributeString(Int32) Retrieve the value of the specified attribute from the native C implementation.  
Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025