Keysight VISA.NET Help
SetAttributeString Method (INativeVisaSession)



Set the value of the specified attribute in the underlying VISA C implementation.
Overload List
OverloadDescription
SetAttributeString(NativeVisaAttribute,String) Set the value of the specified attribute in the underlying VISA C implementation.  
SetAttributeString(Int32,String) Set the value of the specified attribute in the underlying VISA C implementation.  
Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025