| Ivi.Visa Namespace > IPxiBackplaneSession Interface : UnmapTrigger Method |
| Overload | Description |
|---|---|
| UnmapTrigger(Int16,TriggerLine) | Unmap all destination trigger lines to which the specified source trigger line is currently connected. |
| UnmapTrigger(Int16,TriggerLine,Int16,TriggerLine) | Unmap the specified source trigger line from the specified destination trigger line. |
Current with Keysight IO Libraries Suite 18