Keysight VISA.NET Help
HiSLIPOverlapEnabled Property (ITcpipSession)



Specifies whether the HiSLIP "overlap" mode is enabled.
Syntax
'Declaration
 
Property HiSLIPOverlapEnabled As Boolean
'Usage
 
Dim instance As ITcpipSession
Dim value As Boolean
 
instance.HiSLIPOverlapEnabled = value
 
value = instance.HiSLIPOverlapEnabled
bool HiSLIPOverlapEnabled {get; set;}
property bool HiSLIPOverlapEnabled {
   bool get();
   void set (    bool value);
}
Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025