Keysight VISA.NET Help
ChassisLogicalAddress Property (IVxiSession)



The logical address of a given device in the mainframe that serves as a unique ID for the mainframe.
Syntax
'Declaration
 
ReadOnly Property ChassisLogicalAddress As Short
'Usage
 
Dim instance As IVxiSession
Dim value As Short
 
value = instance.ChassisLogicalAddress
short ChassisLogicalAddress {get;}
property short ChassisLogicalAddress {
   short get();
}
Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025