Keysight VISA.NET Help
IsImmediateServant Property (IVxiSession)



If true, the device is an immediate servant of the controller running VISA.
Syntax
'Declaration
 
ReadOnly Property IsImmediateServant As Boolean
'Usage
 
Dim instance As IVxiSession
Dim value As Boolean
 
value = instance.IsImmediateServant
bool IsImmediateServant {get;}
property bool IsImmediateServant {
   bool get();
}
Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025