Keysight VISA.NET Help
GetMacroNameFromStatusCode Method



Returns the VISA name of the specified VISA defined error status code, without the leading "VI_".
Syntax
'Declaration
 
Public Shared Function GetMacroNameFromStatusCode( _
   ByVal status As Integer _
) As String
'Usage
 
Dim status As Integer
Dim value As String
 
value = NativeErrorCode.GetMacroNameFromStatusCode(status)
public static string GetMacroNameFromStatusCode( 
   int status
)
public:
static String^ GetMacroNameFromStatusCode( 
   int status
) 

Parameters

status
Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025