Keysight VISA.NET Help
Inequality Operator



The first ParseResult
The second ParseResult
Returns True iff the two ParseResult objects are not equivalent. Two ParseResult objects are equivalent if the ExpandedUnaliasedName for the two objects have the same value with their case ignored.
Syntax
'Declaration
 
Public Operator <>( _
   ByVal parse1 As ParseResult, _
   ByVal parse2 As ParseResult _
) As Boolean
'Usage
 
public bool operator !=( 
   ParseResult parse1,
   ParseResult parse2
)
public:
bool operator !=( 
   ParseResult^ parse1,
   ParseResult^ parse2
)

Parameters

parse1
The first ParseResult
parse2
The second ParseResult
Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025