| Ivi.Visa Namespace : VisaConstants Class |
For a list of all members of this type, see VisaConstants members.
| Name | Description | |
|---|---|---|
![]() | GpibNoSecondaryAddress | For GPIB resources, this value indicates that there is no secondary address. Actual secondary address values are in the range 0-30 inclusive. |
![]() | ImmediateTimeout | Specifies an immediate timeout, for use with method overloads where the timeout is specified in milliseconds. If the operation cannot be satisfied immediately, it throws a timeout exception rather than blocking. |
![]() | InfiniteTimeout | Specifies an infinite timeout, for use with method overloads where the timeout is specified in milliseconds. |
![]() | UnknownSlotNumber | For PXI and VXI resources, this value indicates that the slot number is unknown or not applicable. |
![]() | VxiUnknownLogicalAddress | For VXI and VME resources, this value indicates that the logical address is unknown or not applicable. |