Keysight VISA.NET Help
VisaException Constructor(SerializationInfo,StreamingContext)



The System.Runtime.Serialization.SerializationInfo that holds the serialized object data about the exception being thrown.
The System.Runtime.Serialization.StreamingContext that contains contextual information about the source or destination.
Initializes a new instance of the VisaException class with serialized data.
Syntax
'Declaration
 
Protected Function New( _
   ByVal info As SerializationInfo, _
   ByVal context As StreamingContext _
)
'Usage
 
Dim info As SerializationInfo
Dim context As StreamingContext
 
Dim instance As New VisaException(info, context)
protected VisaException( 
   SerializationInfo info,
   StreamingContext context
)
protected:
VisaException( 
   SerializationInfo^ info,
   StreamingContext context
)

Parameters

info
The System.Runtime.Serialization.SerializationInfo that holds the serialized object data about the exception being thrown.
context
The System.Runtime.Serialization.StreamingContext that contains contextual information about the source or destination.
Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025