Keysight VISA.NET Help
VxiInterruptEventArgs Class Members
Properties 


The following tables list the members exposed by VxiInterruptEventArgs.

Public Constructors
 NameDescription
Public ConstructorVxiInterruptEventArgs ConstructorInitializes a new instance of the VxiInterruptEventArgs class.  
Top
Public Properties
 NameDescription
Public PropertyCustomEventType A value that uniquely identifies an implementation-specific event type. (Inherited from Ivi.Visa.VisaEventArgs)
Public PropertyEventType The VISA.NET standard event type. (Inherited from Ivi.Visa.VisaEventArgs)
Public PropertyIrqLevel The interrupt level of the VXI VME interrupt.  
Public PropertyStatusId The status ID of the VXI VME interrupt.  
Top
See Also

Reference

VxiInterruptEventArgs Class
Ivi.Visa Namespace

 

 


© Keysight Technologies 2015-2025