Keysight VISA.NET Help
GpibInterfaceSession Class Methods


For a list of all members of this type, see GpibInterfaceSession members.

Public Methods
 NameDescription
Public MethodAssertTrigger Asserts a software trigger.  
Public MethodControlAtn Controls the state of the GPIB ATN interface line, and optionally the active controller state of the local interface board.  
Public MethodDisableEventDisables a calling program's ability to receive events of the type specified by the eventType argument using a VisaSession.WaitOnEvent method (any overload). (Inherited from Keysight.Visa.VisaSession)
Public MethodDiscardEventsDiscards events of the type specified by the eventType argument from the queue for that event type. (Inherited from Keysight.Visa.VisaSession)
Public MethodDisposeOverloaded.  Performs tasks associated with freeing, releasing, or resetting unmanaged VISA resources used by this session. (Inherited from Keysight.Visa.VisaSession)
Public MethodEnableEventEnables a calling program's ability to receive events of the type specified by the eventType argument using a WaitOnEvent method. (Inherited from Keysight.Visa.VisaSession)
Public MethodLockResourceOverloaded.  Acquires a lock on the resource for this session. (Inherited from Keysight.Visa.VisaSession)
Public MethodPassControlOverloaded.  Tells the GPIB device at the specified address to become controller in charge (CIC).  
Public MethodSendCommand Writes GPIB command bytes on the bus.  
Public MethodSendInterfaceClear Pulses the interface clear line (IFC) for at least 100 microseconds. This operation asserts the IFC line and the local interface becomes controller in charge (CIC).  
Public MethodSendRemoteLocalCommand Controls the state of the GPIB REN interface line and, optionally, the remote/local state of the device.  
Public MethodUnlockResource Unlocks the resource. (Inherited from Keysight.Visa.VisaSession)
Public MethodWaitOnEventOverloaded.  Waits for an occurrence of the specified event for this session. In particular, WaitOnEvent suspends execution of the thread on which it is called and waits for the specified event indefinitely. (Inherited from Keysight.Visa.VisaSession)
Top
Protected Methods
 NameDescription
Protected MethodFinalize Performs tasks associated with freeing, releasing, or resetting unmanaged VISA resources used by this session. (Inherited from Keysight.Visa.VisaSession)
Top
See Also

Reference

GpibInterfaceSession Class
Keysight.Visa Namespace

 

 


© Keysight Technologies 2015-2025