Keysight VISA.NET Help
TerminationCharacterEnabled Property (GpibInterfaceSession)



If true, a raw I/O read operation ends when a termination character is received.
Syntax
'Declaration
 
Public Property TerminationCharacterEnabled As Boolean
'Usage
 
Dim instance As GpibInterfaceSession
Dim value As Boolean
 
instance.TerminationCharacterEnabled = value
 
value = instance.TerminationCharacterEnabled
public bool TerminationCharacterEnabled {get; set;}
public:
property bool TerminationCharacterEnabled {
   bool get();
   void set (    bool value);
}
Remarks

The default is false.

Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025