Keysight VISA.NET Help
SetAttributeBoolean Method (IKeysightInternalResourceManager)



The specified attribute ID.
The value to which the attribute will be set.
Set the boolean value of the specified attribute in the underlying VISA C implementation.
Syntax
'Declaration
 
Sub SetAttributeBoolean( _
   ByVal attribute As Integer, _
   ByVal value As Boolean _
) 
'Usage
 
Dim instance As IKeysightInternalResourceManager
Dim attribute As Integer
Dim value As Boolean
 
instance.SetAttributeBoolean(attribute, value)
void SetAttributeBoolean( 
   int attribute,
   bool value
)
void SetAttributeBoolean( 
   int attribute,
   bool value
) 

Parameters

attribute
The specified attribute ID.
value
The value to which the attribute will be set.
Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025