Keysight VISA.NET Help
TerminationCharacterEnabled Property (MessageBasedSession)



If true, read operations end when a termination character is received. This property applies to this session only (VISA local scope).
Syntax
'Declaration
 
Public Property TerminationCharacterEnabled As Boolean
'Usage
 
Dim instance As MessageBasedSession
Dim value As Boolean
 
instance.TerminationCharacterEnabled = value
 
value = instance.TerminationCharacterEnabled
public bool TerminationCharacterEnabled {get; set;}
public:
property bool TerminationCharacterEnabled {
   bool get();
   void set (    bool value);
}
Remarks

The default is false.

Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025