Keysight VISA.NET Help
VisaFrameworkPath Property



The full pathname of the VISA Framework directory used by this implementation of Keysight VISA.NET. The pathname returned varies, depending on whether the process is a 32-bit or 64-bit process. (Keysight Specific)
Syntax
'Declaration
 
Public ReadOnly Property VisaFrameworkPath As String
'Usage
 
Dim instance As ResourceManager
Dim value As String
 
value = instance.VisaFrameworkPath
public string VisaFrameworkPath {get;}
public:
property String^ VisaFrameworkPath {
   String^ get();
}
Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025