Keysight VISA.NET Help
ServerCertificateIsPerpetual Property (TcpipSession)



Indicates the certificate does not expire. Note that this may indicate that the certificate is from an IDevID.
Syntax
'Declaration
 
Public ReadOnly Property ServerCertificateIsPerpetual As Boolean
'Usage
 
Dim instance As TcpipSession
Dim value As Boolean
 
value = instance.ServerCertificateIsPerpetual
public bool ServerCertificateIsPerpetual {get;}
public:
property bool ServerCertificateIsPerpetual {
   bool get();
}
Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025