Keysight VISA.NET Help
ControlOut Method (UsbSession)



Sends arbitrary data to a USB device on the default control port.
Overload List
OverloadDescription
ControlOut(Int16,Int16,Int16,Int16) Sends arbitrary data to a USB device on the default control port.  
ControlOut(Int16,Int16,Int16,Int16,Byte[]) Sends arbitrary data to a USB device on the default control port.  
Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025