| Keysight.Visa Namespace > UsbSession Class : ManufacturerName Property |
'DeclarationPublic ReadOnly Property ManufacturerName As String
'UsageDim instance As UsbSession Dim value As String value = instance.ManufacturerName
public string ManufacturerName {get;}
When using multiple implementations of VISA.NET from different vendors, the value of this attribute should be used for display purposes only and not for programmatic decisions, as the value can be different between VISA implementations and/or revisions.
Current with Keysight IO Libraries Suite 18