Keysight VISA.NET Help
UsbSerialNumber Property (UsbSession)



The serial number of the USB device.
Syntax
'Declaration
 
Public ReadOnly Property UsbSerialNumber As String
'Usage
 
Dim instance As UsbSession
Dim value As String
 
value = instance.UsbSerialNumber
public string UsbSerialNumber {get;}
public:
property String^ UsbSerialNumber {
   String^ get();
}
Remarks

The value of this attribute should be used for display purposes only and not for programmatic decisions.

Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025