Keysight VISA.NET Help
MemorySpace Property (VxiSession)



[Register-Based] The VXIbus address space used by the device.
Syntax
'Declaration
 
Public ReadOnly Property MemorySpace As AddressSpace
'Usage
 
Dim instance As VxiSession
Dim value As AddressSpace
 
value = instance.MemorySpace
public AddressSpace MemorySpace {get;}
public:
property AddressSpace MemorySpace {
   AddressSpace get();
}
Remarks

The default is AddressSpace.VxiA16.

Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025