GPIB Bus Interface (INTFC) Resource
This topic describes the GPIB Bus Interface (INTFC) Resource that is provided to encapsulate the operations and properties of a raw GPIB interface (reading, writing, triggering, etc.).
INTFC Resource Overview
A VISA GPIB Bus Interface (INTFC) Resource, like any other resource, defines the basic operations and attributes of the VISA Resource Template.
For example, modifying the state of an attribute is done via the operation viSetAttribute. Although the INTFC resource does not have viSetAttribute listed in its operations, it provides the operation because it is defined in the VISA Resource Template. From this basic set, each resource adds its specific operations and attributes that allow it to perform its dedicated task.
The INTFC Resource lets a controller interact with any devices connected to the board associated with this resource. Services are provided to send blocks of data onto the bus, request blocks of data from the bus, trigger devices on the bus, and send miscellaneous commands to any or all devices. In addition, the controller can directly query and manipulate specific lines on the bus and also pass control to other devices with controller capability.
INTFC Resource Attributes
|
Attribute Name |
Attribute Value |
Access Privileges |
Data Type |
Range |
Default |
|
|---|---|---|---|---|---|---|
Generic INTFC Resource Attributes |
||||||
| 0x3FFF0189UL |
RW |
Global |
ViUInt8 |
0 to FFh |
N/A |
|
| 0x3FFF001EUL |
RW |
Local |
ViBoolean |
VI_TRUE |
VI_TRUE |
|
| 0x3FFF0192UL |
RW |
Local |
ViBoolean |
VI_TRUE |
VI_FALSE |
|
| 0xBFFF00E9UL |
RO |
Global |
ViString |
N/A |
N/A |
|
| 0x3FFF0176UL |
RO |
Global |
ViUInt16 |
0 to FFFFh |
0 |
|
| 0x3FFF0171UL |
RO |
Global |
ViUInt16 |
VI_INTF_GPIB |
VI_INTF_GPIB |
|
| 0x3FFF002AUL |
RW |
Local |
ViUInt16 |
VI_FLUSH_ON_ACCESS |
VI_FLUSH_ |
|
| 0x3FFF0016UL |
RW |
Local |
ViBoolean |
VI_TRUE |
VI_TRUE |
|
| 0x3FFF0018UL |
RW |
Local |
ViUInt8 |
0 to FFh |
0Ah (linefeed) |
|
| 0x3FFF0038UL |
RW |
Local |
ViBoolean |
VI_TRUE |
VI_FALSE |
|
| 0x3FFF001AUL |
RW |
Local |
ViUInt32 |
VI_TMO_IMMEDIATE |
2000 msec |
|
| 0x3FFF002DUL |
RW |
Local |
ViUInt16 |
VI_FLUSH_ON_ACCESS |
VI_FLUSH_WHEN_FULL |
|
| 0x3FFF002BUL |
RO |
Local |
ViUInt32 |
N/A |
N/A |
|
| 0x3FFF002EUL |
RO |
Local |
ViUInt32 |
N/A |
N/A |
|
GPIB-Specific INTFC Resource Attributes |
||||||
| 0x3FFF005CUL |
RO |
Global |
ViInt16 |
VI_GPIB_UNADDRESSED |
N/A |
|
| 0x3FFF0069UL |
RW |
Global |
ViInt16 |
1 to 15 |
N/A |
|
| 0x3FFF0173UL |
RW |
Global |
ViUInt16 |
0 to 30 |
VI_NO_SEC_ADDR |
|
| 0x3FFF0057UL |
RO |
Global |
ViInt16 |
VI_STATE_ASSERTED |
N/A |
|
| 0x3FFF005EUL |
RO |
Global |
ViBoolean |
VI_TRUE |
N/A |
|
| 0x3FFF0062UL |
RO |
Global |
ViInt16 |
VI_STATE_ASSERTED |
N/A |
|
| 0x3FFF0172UL |
RW |
Global |
ViUInt16 |
0 to 30 |
N/A |
|
| 0x3FFF0181UL |
RO |
Global |
ViInt16 |
VI_STATE_ASSERTED |
N/A |
|
| 0x3FFF0067UL |
RO |
Global |
ViInt16 |
VI_STATE_ASSERTED |
N/A |
|
| 0x3FFF0068UL |
RW |
Global |
ViBoolean |
VI_TRUE |
N/A |
|
INTFC Resource Attribute Descriptions
|
Attribute Name |
Attribute Value |
Description |
|---|---|---|
Generic INTFC Resource Attributes |
||
|
VI_ATTR_INTF_NUM |
0x3FFF0176UL |
Board number for the given interface. |
|
VI_ATTR_INTF_TYPE |
0x3FFF0171UL |
Interface type of the given session. |
|
VI_ATTR_INTF_INST_NAME |
0xBFFF00E9UL |
Human-readable text describing the given interface. |
|
VI_ATTR_SEND_END_EN |
0x3FFF0016UL |
Whether to assert END during the transfer of the last byte of the buffer. |
|
VI_ATTR_TERMCHAR |
0x3FFF0018UL |
Termination character. When the termination character is read and VI_ATTR_TERMCHAR_EN is enabled during a read operation, the read operation terminates. |
|
VI_ATTR_TERMCHAR_EN |
0x3FFF0038UL |
Flag that determines whether the read operation should terminate when a termination character is received. |
|
VI_ATTR_TMO_VALUE |
0x3FFF001AUL |
Minimum timeout value to use, in milliseconds. A timeout value of VI_TMO_IMMEDIATE means that operations should never wait for the device to respond. A timeout value of VI_TMO_INFINITE disables the timeout mechanism. |
|
VI_ATTR_DEV_STATUS_BYTE |
0x3FFF0189UL |
This attribute specifies the 488-style status byte of the local controller associated with this session. If this attribute is written and bit 6 (0x40) is set, this device or controller will assert a service request (SRQ) if it is defined for this interface. |
|
VI_ATTR_WR_BUF_OPER_MODE |
0x3FFF002DUL |
Determines the operational mode of the write buffer. When the operational mode is set to VI_FLUSH_WHEN_FULL (default), the buffer is flushed when an END indicator is written to the buffer, or when the buffer fills up. If the operational mode is set to VI_FLUSH_ON_ACCESS, the write buffer is flushed under the same conditions, and also every time a viPrintf operation completes. |
|
VI_ATTR_DMA_ALLOW_EN |
0x3FFF001EUL |
This attribute specifies whether I/O accesses should use DMA ( VI_TRUE) or Programmed I/O ( VI_FALSE). In some implementations, this attribute may have global effects even though it is documented to be a local attribute. Since this affects performance and not functionality, that behavior is acceptable. |
|
VI_ATTR_RD_BUF_OPER_MODE |
0x3FFF002AUL |
Determines the operational mode of the read buffer. When the operational mode is set to VI_FLUSH_DISABLE (default), the buffer is flushed only on explicit calls to viFlush. If the operational mode is set to VI_FLUSH_ON_ACCESS, the buffer is flushed every time a viScanf operation completes. |
|
VI_ATTR_FILE_APPEND_EN |
0x3FFF0192UL |
This attribute specifies whether viReadToFile will overwrite (truncate) or append when opening a file. |
|
VI_ATTR_RD_BUF_SIZE |
0x3FFF002BUL |
This attribute specifies the size of the formatted I/O read buffer. The user can modify this value by calling viSetBuf(). |
|
VI_ATTR_WR_BUF_SIZE |
0x3FFF002EUL |
This attribute specifies the size of the formatted I/O write buffer. The user can modify this value by calling viSetBuf(). |
GPIB-Specific INTFC Resource Attributes |
||
|
VI_ATTR_GPIB_PRIMARY_ADDR |
0x3FFF0172UL |
Primary address of the local GPIB controller used by the given session. |
|
VI_ATTR_GPIB_SECONDARY_ADDR |
0x3FFF0173UL |
Secondary address of the local GPIB controller used by the given session. |
|
VI_ATTR_GPIB_REN_STATE |
0x3FFF0181UL |
This attribute returns the current state of the GPIB REN (Remote ENable) interface line. |
|
VI_ATTR_GPIB_ATN_STATE |
0x3FFF0057UL |
This attribute shows the current state of the GPIB ATN (ATtentioN) interface line. |
|
VI_ATTR_GPIB_NDAC_STATE |
0x3FFF0062UL |
This attribute shows the current state of the GPIB NDAC
|
|
VI_ATTR_GPIB_SRQ_STATE |
0x3FFF0067UL |
This attribute shows the current state of the GPIB SRQ (Service ReQuest) interface line. |
|
VI_ATTR_GPIB_CIC_STATE |
0x3FFF005EUL |
This attribute shows whether the specified GPIB interface is currently CIC (controller in charge). |
|
VI_ATTR_GPIB_SYS_CNTRL_STATE |
0x3FFF0068UL |
This attribute shows whether the specified GPIB interface is currently the system controller. In some implementations, this attribute may be modified only through a configuration utility. On these systems, this attribute is read only (RO). |
|
VI_ATTR_GPIB_HS488_CBL_LEN |
0x3FFF0069UL |
This attribute specifies the total number of meters of GPIB cable used in the specified GPIB interface. If HS488 is not implemented, querying this attribute should return the value VI_GPIB_HS488_NIMPL. On these systems, trying to set this attribute value will return error VI_ERROR_NSUP_ATTR_STATE. |
|
VI_ATTR_GPIB_ADDR_STATE |
0x3FFF005CUL |
This attribute shows whether the specified GPIB interface is currently addressed to talk or listen, or is not addressed. |
INTFC Resource Events
This resource defines the following events for communication with applications, where AP = Access Privilege.
VI_EVENT_GPIB_CIC - Notification that the GPIB controller has gained or lost CIC (controller in charge) status.
|
Event Attribute |
Attribute Value |
Description |
AP |
Data Type |
Range |
|---|---|---|---|---|---|
| 0x3FFF4010UL |
Unique logical identifier of the event. |
RO |
ViEventType |
VI_EVENT_GPIB_CIC |
|
| 0x3FFF4193UL |
Controller has become controller in charge. |
RO |
ViBoolean |
VI_TRUE |
VI_EVENT_GPIB_TALK - Notification that the GPIB controller has been addressed to talk.
|
Event Attribute |
Attribute Value |
Description |
AP |
Data Type |
Range |
|---|---|---|---|---|---|
|
VI_ATTR_EVENT_TYPE |
0x3FFF4010UL |
Unique logical identifier of the event. |
RO |
ViEventType |
VI_EVENT_GPIB_TALK |
VI_EVENT_GPIB_LISTEN - Notification that the GPIB controller has been addressed to listen.
|
Event Attribute |
Attribute Value |
Description |
AP |
Data Type |
Range |
|---|---|---|---|---|---|
|
VI_ATTR_EVENT_TYPE |
0x3FFF4010UL |
Unique logical identifier of the event. |
RO |
ViEventType |
VI_EVENT_GPIB_LISTEN |
VI_EVENT_CLEAR - Notification that the GPIB controller has been sent a device clear message.
|
Event Attribute |
Attribute Value |
Description |
AP |
Data Type |
Range |
|---|---|---|---|---|---|
| 0x3FFF4010UL |
Unique logical identifier of the event. |
RO |
ViEventType |
VI_EVENT_CLEAR |
VI_EVENT_TRIG - Notification that a trigger interrupt was received from the interface.
|
Event Attribute |
Attribute Value |
Description |
AP |
Data Type |
Range |
|---|---|---|---|---|---|
|
VI_ATTR_EVENT_TYPE |
0x3FFF4010UL |
Unique logical identifier of the event. |
RO |
ViEventType |
VI_EVENT_TRIG |
| 0x3FFF4012UL |
The identifier of the triggering mechanism on which the specified trigger event was received. |
RO |
ViInt16 |
VI_TRIG_SW |
VI_EVENT_IO_COMPLETION - Notification that an asynchronous operation has completed.
|
Event Attribute |
Attribute Value |
Description |
AP |
Data Type |
Range |
|---|---|---|---|---|---|
| 0x3FFF4010UL |
Unique logical identifier of the event. |
RO |
ViEventType |
VI_EVENT_IO_COMPLETION |
|
| 0x3FFF4025UL |
Return code of the asynchronous I/O operation that has completed. |
RO |
ViStatus |
N/A |
|
| 0x3FFF4006UL |
Job ID of the asynchronous operation that has completed. |
RO |
ViJobId |
N/A |
|
| 0x3FFF4027UL |
Address of buffer used in an asynchronous operation. |
RO |
ViBuf |
N/A |
|
|
32-bit: 0x3FFF4026UL 64-bit: 0x3FFF4028UL |
Actual number of elements that were asynchronously transferred. |
RO |
ViBus Size |
* |
|
| 0x3FFF4026UL |
Actual number of elements that were asynchronously transferred. |
RO |
ViUInt32 |
0 to FFFFFFFFh |
|
| 0x3FFF4028UL |
Actual number of elements that were asynchronously transferred. |
RO |
ViUInt64 |
0 to FFFFFFFF FFFFFFFFh |
|
| 0xBFFF4042UL |
The name of the operation generating the event. |
RO |
ViString |
N/A |
*The data type is defined in the appropriate VPP 4.3.x framework specification.
**Defined only for operating systems that are 64-bit native.
INTFC Resource Operations
viAssertTrigger (vi, protocol)
viBufRead (vi, buf, count, retCount)
viBufWrite (vi, buf, count, retCount)
viGpibCommand (vi, buf, count, retCount)
viGpibPassControl (vi, primAddr, secAddr)
viPrintf (vi, writeFmt, arg1, arg2, ...)
viRead (vi, buf, count, retCount)
viReadAsync (vi, buf, count, jobId)
viReadToFile (vi, fileName, count, retCount)
viScanf (vi, readFmt, arg1, arg2, ...)
viSPrintf (vi, buf, writeFmt, arg1, arg2, ...)
viSScanf (vi, buf, readFmt, arg1, arg2, ...)
viVPrintf (vi, writeFmt, params)
viVScanf (vi, readFmt, params)
viVSPrintf (vi, buf, writeFmt, params)
viVSScanf (vi, buf, readFmt, params)
viWrite (vi, buf, count, retCount)
viWriteAsync (vi, buf, count, jobId)
viWriteFromFile (vi, fileName, count, retCount)