viBufWrite
Syntax
viBufWrite(ViSession vi, ViBuf buf, ViUInt32 count, ViPUInt32 retCount);
Description
Similar to viWrite, except the data is written to the formatted I/O write buffer rather than directly to the device. This operation is similar to viWrite and does not perform any kind of data formatting. It differs from viWrite in that the data is written to the formatted I/O write buffer (the same buffer as used by viPrintf and related operations) rather than directly to the device. This operation can intermix with the viPrintf operation, but mixing it with the viWrite operation is discouraged.
If you pass VI_NULL as the retCount parameter to the viBufWrite operation, the number of bytes transferred will not be returned. This may be useful if it is important to know only whether the operation succeeded or failed.
Parameters
| 
                                                     Name  | 
                                                
                                                     Dir  | 
                                                
                                                     Type  | 
                                                
                                                     Description  | 
                                            
|---|---|---|---|
| 
                                                     vi  | 
                                                
                                                     IN  | 
                                                
                                                     ViSession  | 
                                                
                                                     Unique logical identifier to a session.  | 
                                            
| 
                                                     buf  | 
                                                
                                                     IN  | 
                                                
                                                     ViBuf  | 
                                                
                                                     Represents the location of a data block to be sent to the device.  | 
                                            
| 
                                                     count  | 
                                                
                                                     IN  | 
                                                
                                                     ViUInt32  | 
                                                
                                                     Number of bytes to be written.  | 
                                            
| 
                                                     retCount  | 
                                                
                                                     OUT  | 
                                                
                                                     ViPUInt32  | 
                                                
                                                     Represents the location of an integer that will be set to the number of bytes actually transferred.  | 
                                            
                                                    Special Values for retCount Parameter | 
                                            |||
| 
                                                     Value  | 
                                                
                                                     
  | 
                                                
                                                     
  | 
                                                
                                                     Action Description  | 
                                            
| 
                                                     VI_NULL  | 
                                                
                                                     
  | 
                                                
                                                     
  | 
                                                
                                                     Do not return the number of bytes transferred.  | 
                                            
Return Values
| 
                                                     Type ViStatus  | 
                                                
                                                     This is the function return status. It returns either a completion code or an error code as follows.  | 
                                            
| 
                                                     Completion Code  | 
                                                
                                                     Description  | 
                                            
|---|---|
| 
                                                     VI_SUCCESS  | 
                                                
                                                     Operation completed successfully.  | 
                                            
| 
                                                     Error Code  | 
                                                
                                                     Description  | 
                                            
| 
                                                     VI_ERROR_INV_SESSION  | 
                                                
                                                     The given session or object reference is invalid (both are the same value).  | 
                                            
| 
                                                     VI_ERROR_INV_SETUP  | 
                                                
                                                     Unable to start write operation because setup is invalid (due to attributes being set to an inconsistent state).  | 
                                            
| 
                                                     VI_ERROR_IO  | 
                                                
                                                     An unknown I/O error occurred during transfer.  | 
                                            
| 
                                                     VI_ERROR_NSUP_OPER  | 
                                                
                                                     The given vi does not support this function.  | 
                                            
| 
                                                     VI_ERROR_RSRC_LOCKED  | 
                                                
                                                     Specified operation could not be performed because the resource identified by vi has been locked for this kind of access.  | 
                                            
| 
                                                     VI_ERROR_TMO  | 
                                                
                                                     Timeout expired before function completed.  |