viGpibControlREN
Syntax
viGpibControlREN(ViSession vi, ViUInt16 mode);
Description
Controls the state of the GPIB REN interface line and, optionally, the remote/local state of the device. This operation asserts or deasserts the GPIB REN interface line according to the specified mode. The mode can also specify whether the device associated with this session should be placed in local state (before deasserting REN) or remote state (after asserting REN). This operation is valid only if the GPIB interface associated with the session specified by vi is currently the system controller.
An INSTR resource implementation of viGpibControlREN for a GPIB System supports all documented modes. An INTFC resource implementation of viGpibControlREN for a GPIB System supports the modes VI_GPIB_REN_DEASSERT, VI_GPIB_REN_ASSERT, and VI_GPIB_REN_ASSERT_LLO.
Parameters
| 
                                                     Name  | 
                                                
                                                     Dir  | 
                                                
                                                     Type  | 
                                                
                                                     Description  | 
                                            
|---|---|---|---|
| 
                                                     vi  | 
                                                
                                                     IN  | 
                                                
                                                     ViSession  | 
                                                
                                                     Unique logical identifier to a session.  | 
                                            
| 
                                                     mode  | 
                                                
                                                     IN  | 
                                                
                                                     ViUInt16  | 
                                                
                                                     Specifies the state of the REN line and, optionally, the device remote/local state.  | 
                                            
                                                    Special Values for mode Parameter | 
                                            |||
| 
                                                     mode  | 
                                                
                                                     Action Description  | 
                                            ||
| 
                                                     VI_GPIB_REN_ADDRESS_GTL  | 
                                                
                                                     
  | 
                                                
                                                     
  | 
                                                
                                                     Send the Go To Local command (GTL) to this device.  | 
                                            
| 
                                                     VI_GPIB_REN_ASSERT  | 
                                                
                                                     
  | 
                                                
                                                     
  | 
                                                
                                                     Assert REN line.  | 
                                            
| 
                                                     VI_GPIB_REN_ASSERT_ADDRESS_LLO  | 
                                                
                                                     
  | 
                                                
                                                     
  | 
                                                
                                                     Address this device and send it LLO, putting it in RWLS.  | 
                                            
| 
                                                     VI_GPIB_REN_ASSERT_ADDRESS  | 
                                                
                                                     
  | 
                                                
                                                     
  | 
                                                
                                                     Assert REN line and address this device.  | 
                                            
| 
                                                     VI_GPIB_REN_ASSERT_LLO  | 
                                                
                                                     
  | 
                                                
                                                     
  | 
                                                
                                                     Send LLO to any devices that are addressed to listen.  | 
                                            
| 
                                                     VI_GPIB_REN_DEASSERT  | 
                                                
                                                     
  | 
                                                
                                                     
  | 
                                                
                                                     Deassert REN line.  | 
                                            
| 
                                                     VI_GPIB_REN_DEASSERT_GTL  | 
                                                
                                                     
  | 
                                                
                                                     
  | 
                                                
                                                     Send the Go To Local command (GTL) to this device and deassert REN line.  | 
                                            
Return Values
| 
                                                     Type ViStatus  | 
                                                
                                                     This is the function return status. It returns either a completion code or an error code as follows.  | 
                                            
| 
                                                     Completion Code  | 
                                                
                                                     Description  | 
                                            
|---|---|
| 
                                                     VI_SUCCESS  | 
                                                
                                                     Resource attribute retrieved successfully.  | 
                                            
| 
                                                     Error Code  | 
                                                
                                                     Description  | 
                                            
| 
                                                     VI_ERROR_INV_MODE  | 
                                                
                                                     The value specified by the mode parameter is invalid.  | 
                                            
| 
                                                     VI_ERROR_INV_SESSION  | 
                                                
                                                     The given session or object reference is invalid (both are the same value).  | 
                                            
| 
                                                     VI_ERROR_NCIC  | 
                                                
                                                     The interface associated with this session is not currently the controller in charge.  | 
                                            
| 
                                                     VI_ERROR_NLISTENERS  | 
                                                
                                                     No listeners condition is detected (both NRFD and NDAC are deasserted).  | 
                                            
| 
                                                     VI_ERROR_NSUP_OPER  | 
                                                
                                                     The given vi does not support this operation.  | 
                                            
| 
                                                     VI_ERROR_NSYS_CNTLR  | 
                                                
                                                     The interface associated with this session is not the system controller.  | 
                                            
| 
                                                     VI_ERROR_RSRC_LOCKED  | 
                                                
                                                     Specified operation could not be performed because the resource identified by vi has been locked for this kind of access.  |