viMapAddress

This section contains information specific to the Windows product.

Syntax

viMapAddress(ViSession vi, ViUInt16 mapSpace, ViBusAddress mapBase , ViBusSize mapSize, ViBoolean access, ViAddr suggested, ViPAddr address);

Description

This function maps in a specified memory space. The memory space that is mapped is dependent on the type of interface specified by the vi parameter and the mapSpace parameter (see the following table). The address parameter returns the address in your process space where memory is mapped. The values for the mapSpace parameter are:

Value

Description

VI_A16_SPACE

Map the A16 address space of VXI/MXI bus.

VI_A24_SPACE

Map the A24 address space of VXI/MXI bus.

VI_A32_SPACE

Map the A32 address space of VXI/MXI bus.

VI_A64_SPACE

Address the A64 address space of VXI/MXI bus.

VI_PXI_CFG_SPACE

Address the PCI configuration space.

VI_PXI_BAR0_SPACE – VI_PXI_BAR5_SPACE

Address the specified PCI memory or I/O space.

VI_PXI_ALLOC_SPACE

Access physical locally allocated memory.

  • If the viSession parameter (vi) refers to an INSTR session, the mapBase parameter specifies a relative offset in the instrument’s mapSpace. If the ViSession parameter (vi) refers to a MEMACC session, the mapBase parameter is an absolute offset from the start of the VXI mapSpace.

For a given session, you can only have one map at one time. If you need to have multiple maps to a device, you must open one session for each map needed.

  • The mapBase parameter specified in the viMapAddress operation for an INSTR resource is the offset address relative to the device's allocated address base for the corresponding address space specified. For example, if mapSpace specifies VI_A16_SPACE, mapBase specifies the offset from the logical address base address of the VXI device specified. If mapSpace specifies VI_A24_SPACE, VI_A32_SPACE, or VI_A64_SPACE, mapBase specifies the offset from the base address of the VXI device's memory space allocated by the VXI Resource Manager within VXI A24, A32, or A64 space.  

  • When calling the viMapAddress function on a PXI session, the maximum value for the mapSize parameter is limited to the actual size of the resource addressed by the mapSpace parameter (VI_PXI_BAR0_SPACE – VI_PXI_BAR5_SPACE).

viMapAddress is not supported for use with VBA on 64-bit systems.

Parameters

Name

Dir

Type

Description

vi

IN

ViSession

Unique logical identifier to a session.

mapSpace

IN

ViUInt16

Specifies the address space to map.

mapBase

IN

ViBusAddress

Offset (in bytes) of the memory to be mapped.

mapSize

IN

ViBusSize

Amount of memory to map (in bytes).

access

IN

ViBoolean

VI_FALSE.

suggested

IN

ViAddr

If suggested parameter is not VI_NULL, the operating system attempts to map the memory to the address specified in suggested. There is no guarantee, however, that the memory will be mapped to that address. This function may map the memory into an address region different from suggested.

address

OUT

ViPAddr

Address in your process space where the memory was mapped.

Return Values

Type ViStatus

This is the function return status. It returns either a completion code or an error code as follows.

Completion Code

Description

VI_SUCCESS

Map successful.

Error Code

Description

VI_ERROR_ALLOC

Unable to allocate window of at least the requested size.

VI_ERROR_INV_ACC_MODE

Invalid access mode.

VI_ERROR_INV_OFFSET

Invalid offset specified.

VI_ERROR_INV_SESSION
VI_ERROR_INV_OBJECT

The given session or object reference is invalid (both are the same value).

VI_ERROR_INV_SETUP

Unable to start operation because the setup is invalid (due to attributes being set to an inconsistent state).

VI_ERROR_INV_SIZE

Invalid size of window specified.

VI_ERROR_INV_SPACE

Invalid mapSpace specified.

VI_ERROR_NSUP_OFFSET

Specified region is not accessible from this hardware.

VI_ERROR_NSUP_OPER

The given vi does not support this operation.

VI_ERROR_RSRC_LOCKED

Specified operation could not be performed because the resource identified by vi has been locked for this kind of access.

VI_ERROR_TMO

viMapAddress could not acquire resource or perform mapping before the timer expired.

VI_ERROR_WINDOW_MAPPED

The specified session already contains a mapped window.

See Also

viUnmapAddress