Start Here: Connectivity Guide

This section of the Keysight IO Libraries Suite Help covers connectivity – connecting instruments to your PC and establishing communication. The basic process for connecting an instrument is:

Start Keysight Connection Expert Classic from IO Control.
Once Connection Expert Classic establishes a connection to each instrument, you can use either Interactive IO Classic or the instrument's Soft Front Panel (SFP) to send commands to and receive data from the instrument.

Interactive IO Classic

Interactive IO is a software utility that lets you interactively send commands to instruments and read the responses without writing any program code. You can use Interactive IO to:

  • Quickly verify connectivity to your instrument
  • Troubleshoot communication problems
  • Become familiar with the instrument's command set
  • Rapidly prototype commands and check the instrument's responses before writing code

Interactive IO contains a number of commonly used commands to simplify communicating with instruments.

Select the instrument that you want to configure. Click the Interactive IO icon in Connection Expert.

Alternately, you can start Interactive IO from Keysight IO Control.

See the Interactive IO Help for usage instructions.

Interactive IO does not operate with PXI (modular) instruments. Windows users with PXI instruments, use the instrument's soft front panel instead of Interactive IO.

Instrument or Chassis Soft Front Panel

Many modular instruments and chassis have Soft Front Panel (SFP) software for monitoring and controlling the instrument or chassis; some have more than one. When installed, the Soft Front Panel software is an interactive user interface for the instrument or chassis. Refer to the instrument's SFP help file for instructions on using the SFP.

Select a chassis in the Chassis Content view, then use the links at the right to start (in a new window) soft front panels for chassis or modules. These links are only shown if a soft front panel is installed for the selected chassis or module. There may be more than one soft front panel for a given module; in that case, each link includes the name and version of the soft front panel to be run.

If a non-Keysight soft front panel is installed in a non-standard location, Connection Expert Classic may not be able to find it. In that case, you will have to locate and run the soft front panel outside of Connection Expert Classic (for example, in Windows Explorer).