Software Revision Matrix

It is generally best to use the current version of the Keysight IO Libraries Suite. The newest version will support the newest interfaces and operating systems, and will have the most advanced features. However, to support an older interface or operating system, you may need to install an earlier version of the IO Libraries Suite.

If you need an earlier version, go to http://www.keysight.com/find/iosuite to locate the version you need.

This table summarizes major revisions of Keysight IO Libraries Suite (previously Agilent IO Libraries Suite), with their supported interfaces and operating systems.

Revisions between 1996 and March 2018 were for Windows only.

IO Libraries Revision

Supported Operating Systems

Supported Interfaces

Changes

IO Libraries Suite 2024 Update (for Windows)
  • Windows 11(64-bit only)
  • Windows 10(64-bit only)
  • Windows 8.1 ((64-bit only))
  • Windows Server 2012 & 2016 (64-bit only)
  • Windows Server 2008 R2 SP1 (64-bit only)
  • USB instruments
  • LAN instruments 3
  • PXI Interface4
  • 82350B/C PCI GPIB Interface
  • 82351A/B PCIe® GPIB Interface
  • 82357A/B USB/GPIB Interface
  • E1406A VXI Command Module (GPIB)5
  • E5810B LAN/GPIB/ USB Gateway
  • E5810A LAN/GPIB Gateway
  • E8491B VXI IEEE 1394 Slot 0(FireWire)5
  • RS-232
Keysight IO Libraries Suite 2024 Update 2:
Enhacement(s):
  • Improved PXI enumeration times on large systems. Systems with multiple chassis, like the six-chassis setup, will now complete PXI enumeration more efficiently, reducing delays caused by repetitive device enumeration during initialization.

  • Added checks for prerequisites in the main IO Libraries Suite (IOLS) installer. This ensures that all necessary dependencies are installed before the main software.

Defect Fixe(s):

  • Fixed an issue where reinstalling the IO Libraries Suite (IOLS) could disrupt other Keysight software, such as the Trigger Manager. The installer now ensures that only IOLS-specific registry entries are updated, preventing the reset of unrelated Keysight Technologies registry entries.

Known Issues

  • Delinea tool for administrator privilege management causes installation, upgrade and uninstallation interference.
  • Upgrading to this version causes loss of previously configured instruments in Connection Expert. Please add those instruments back after installation.
  • Discovery issues with Streamline Series VNAs using both USB or Thunderbolt interfaces.
  • Missing Components in VISA COM Applications

    Ivi.Visa.Interop.dll is missing in the 32-bit VISA COM applications. The workaround to fix the issue is as follows:
    • Install .NET Framework 3.5
    • Uninstall VISA shared component
    • Repair IO Library Suite to install VISA shared component
    Another way to fix the issue is as follows:
    • Open Visual Studio developer command window with elevated privilege
    • Change to C:\Program Files (x86)\IVI Foundation\VISA\VisaCom\Primary Interop Assemblies
    • Run "IviPiaRegistration.bat"
  • Known Issue with Delinea Tool Interference
    • We've identified issues when installing or upgrading IO Libraries Suite (IOLS) on systems where the Delinea tool is used. These issues may include failures during installation or upgrading certain IOLS components.
    • Action Required: If you encounter problems with IOLS installation or upgrades while using Delinea, please get in touch with Keysight Support for assistance.
IO Libraries Suite 2024 Update 1(for Windows)
  • Windows 11(64-bit only)
  • Windows 10(64-bit only)
  • Windows 8.1 ((64-bit only))
  • Windows Server 2012 & 2016 (64-bit only)
  • Windows Server 2008 R2 SP1 (64-bit only)
  • USB instruments
  • LAN instruments 3
  • PXI Interface4
  • 82350B/C PCI GPIB Interface
  • 82351A/B PCIe® GPIB Interface
  • 82357A/B USB/GPIB Interface
  • E1406A VXI Command Module (GPIB)5
  • E5810B LAN/GPIB/ USB Gateway
  • E5810A LAN/GPIB Gateway
  • E8491B VXI IEEE 1394 Slot 0(FireWire)5
  • RS-232
Keysight IO Libraries Suite 2024 Update 1:

New Feature(s):

  • Installation Split into Two Installers

    IO Libraries Suite installation process has undergone a major change. For IO Libraries 2024 Update1 or later, there will be two installers:

    • Prerequisites Installer

      Installs all the necessary dependencies and components that the Keysight IO Libraries Suite requires to function correctly. This might include libraries, drivers, and other software components essential for running the main software.
    • Main Installer
      Installs the primary Keysight IO Libraries Suite software itself. This is the core application that users interact with for their tasks.
      The separate installers allow for more modular installation and easier management of dependencies, potentially reducing the overall installation size and improving flexibility.
      Always start with the prerequisites installer and then proceed with the main installer.
    • Repair Operation

      Re-running the installer will perform a repair operation. There is no explicit “repair” option.
    • Log Files
      The new installer generates multiple log files beginning with ‘kt_’ in the %TEMP% directory. Zip these files for troubleshooting purposes if needed.

  • Anonymous Secure Socket Connection
    IO Libraries 2024 Update 1 introduces secure, encrypted, anonymous communication on a Socket connection.
  • Addition of a new VISA attribute VI_KTATTR_TCPIP_SASL_PASSWORD
    Use this attribute for PLAIN/SCRAM secure Authentication over HiSLIP Connection via Programming.
  • Addition of a New VISA utility

      With IO Libraries Suite 2024 Update 1 onwards, you will not get the option to choose a primary VISA during installation, if another VISA is already present, the installer configures Keysight VISA as a secondary VISA. If no VISA exists, it configures Keysight VISA as the primary VISA. IO Libraries 2024 Update 1 provides a CLI utility that lets you choose a primary VISA anytime. You can access this utility by navigating to the IO Libraries desktop icon, selecting Utilities, and then choosing Set 32-Bit Primary VISA.

      • The utility is for Windows 64-bit OS.
      • It is a CLI application that lists all installed VISA(s) and allows the user to choose the primary VISA interactively or via parameters.
      • The utility should run as admin.
      • The utility handles cases where visa32.dll is used by other applications, prompting userd to close or forcibly terminate them if necessary.
        New Directory for VISA DLLs

      • The utility will use a pre-created folder to store the visa32.dll files from each VISA vendor. Place them at the following location:
        C:\Program Files (x86)\IVI Foundation\VISA\WinNT\visa32Store

NOTE

  • Before starting the installation, you must manually uninstall Keysight IO Libraries Suite versions older than IO Libraries 2024.
  • VXI is not supported on Windows 8 and Windows 11

Known Issues

  • You may need to install .NET Framework 3.5 for 32-bit VISA applications.
  • You can install .NET Framework 3.5 using the IO Libraries Suite installer with the net35 directive. For example: IOLibSuite_version.exe /s /z"typical;net35"
IO Libraries Suite 2024 (for Linux)
  • Red Hat Enterprise Linux Desktop (64-Bit) : 7.4 to 9.0

  • CentOS Linux Desktop (64-Bit): 7.4 to 9.0

  • Ubuntu Desktop (64-Bit): 18.04 to 22.04.2

  • LAN (HiSLIP, VXI-11/SICL-LAN, and SOCKET)
  • PCI/PCIe GPIB,
  • USB/GPIB
  • USBTMC
  • RS-232
  • Remote GPIB
  • Remote USB
  • Remote RS-232

Linux Release IO Libraries Suite 2024 includes the following changes:

 

New Features
  • Added KCCS & KIIS support, services crucial for applications relying on the IO Libraries Suite for instrument discovery and communication. KIIS supports REST communication, while KCCS supports communication via web sockets.

  • KDI utility updated from version 3.2 to 3.4.

IO Libraries Suite 2024 (for Windows)
  • Windows 11
  • Windows 10(64-bit only)
  • Windows Server 2012 & 2016 (64-bit only)
  • Windows Server 2008 R2 SP1 (64-bit only)
  • USB instruments
  • LAN instruments 3
  • PXI Interface4
  • 82350B/C PCI GPIB Interface
  • 82351A/B PCIe® GPIB Interface
  • 82357A/B USB/GPIB Interface
  • E1406A VXI Command Module (GPIB)5
  • E5810B LAN/GPIB/ USB Gateway
  • E5810A LAN/GPIB Gateway
  • E8491B VXI IEEE 1394 Slot 0(FireWire)5
  • RS-232

Keysight IO Libraries Suite 2024:

 

New Feature(s):
  • KDI utility updated from version 3.2 to 3.4

Defect Fixes:

  • Resolved issue related to the M9537A Chassis displaying inaccurate information in the Keysight Connection Expert. The underlying issue, a legacy issue with the M9506A sys module driver, was resolved by assigning the lowest child sys module to the chassis in the cascade relationship.
  • Resolved defect in ktvisa32.cs causing build errors for 32-bit applications in IOLS 2023 and 2023 Update 1. The fix involves changing attribute values to signed 32-bit, ensuring compatibility.
  • Resolved critical defect causing Keysight PSS IC-CAP & WaferPro Express crashes on Linux with PCI-GPIB card.
  • Resolved defect blocking KeyboardInterrupts during USB INSTR sessions. The issue, specific to USB INSTR and caused by a handler problem in the SetConsoleCtrlHandler API, is resolved in this version.
  • Resolved USB plug-and-play detection issue for Argo instruments (N7731C).
IO Libraries Suite 2023 (for Linux)
  • 64-Bit Red Hat Enterprise Linux Desktop: 7.4 to 9.0

  • 64-Bit CentOS Linux Desktop: 7.4 to 9.0

  • 64-Bit Ubuntu Desktop: 18.04 to 22.04.2

  • LAN (HiSLIP, VXI-11/SICL-LAN, and SOCKET)
  • PCI/PCIe GPIB,
  • USB/GPIB
  • USBTMC
  • RS-232
  • Remote GPIB
  • Remote USB
  • Remote RS-232
Linux Release IO Libraries Suite 2023 includes the following changes:

New Features

  • Extended OS Support: Expanded compatibility with a range of Ubuntu, CentOS, and RedHat distributions. Check the System Requirements section for the list of supported versions for each platform.
  • Offline Installation Capability: you can seamlessly install updates on your target system without requiring an internet connection.

Enhancements

  • Enhanced Security with HiSLIP: Added anonymous secure connection support for the HiSLIP interface.
  • Enhanced Performance: Improved the performance of the Format I/O VISA API. Expect faster data transfers and smoother communication with your instruments.

Defect Fixe(s)

  • Resolved the issue causing blank instrument thumbnail images in Connection Expert.
  • Streamlined the IO Monitor by hiding the interface filter.
IO Libraries Suite 2023 Update 1(for Windows)
  • Windows 11
  • Windows 10
  • Windows 8.1
  • Windows 7 SP1
  • Windows Server 2012 & 2016 (64-bit only)
  • Windows Server 2008 R2 SP1 (64-bit only)
  • USB instruments
  • LAN instruments 3
  • PXI Interface4
  • 82350B/C PCI GPIB Interface
  • 82351A/B PCIe® GPIB Interface
  • 82357A/B USB/GPIB Interface
  • E1406A VXI Command Module (GPIB)5
  • E5810B LAN/GPIB/ USB Gateway
  • E5810A LAN/GPIB Gateway
  • E8491B VXI IEEE 1394 Slot 0(FireWire)5
  • RS-232

Keysight IO Libraries Suite 2023 Update 1:

New Feature(s):

  • Introduced KCCS a WebSocket API gateway to the IOLS Discovery Service.
  • Introduced ARM64EC support for IO Libraries Suite VISA
  • Updated KDIC to version 3.2

Defect Fixes:

  • Resolved the issue with viLock failing to maintain an exclusive session lock on PXI instruments. Fixed viUnlock throwing an error (VI_ERROR_SESN_NLOCKED) when the session lock was still active.
  • Resolved the issue with KIIS continuously occupying port numbers in Windows 7 SP1, ensuring proper port management and preventing conflicts with other applications or services.
  • Enhanced performance of VISA-COM APIs for LAN communication.
  • Reduced the processing time taken by the viReadSTB function for USBTMC instruments.
  • Fixed security risk in the electron version of secure-config-client.
  • Fixed the issue related to detecting the visa32.dll file in IOLS 2023.
  • Improved USB-PXI Discovery Server to reduce CPU load.

Note: VXI is not supported on Windows 8 and Windows 11

Known Issues

  • You may need to install .NET Framework 3.5 for 32-bit VISA applications.
  • You can install .NET Framework 3.5 using the IO Libraries Suite installer with the net35 directive. For example: IOLibSuite_version.exe /s /z"typical;net35"
IO Libraries Suite 2023(for Windows)
Windows 11
Windows 10 Windows 8.1 Windows 7 SP1 Windows Server 2012 & 2016 (64-bit only) Windows Server 2008 R2 SP1 (64-bit only)

USB instruments

LAN instruments 3

PXI Interface4

82350B/C PCI GPIB Interface

82351A/B PCIe® GPIB Interface

82357A/B USB/GPIB Interface

E1406A VXI Command Module (GPIB)5

E5810B LAN/GPIB/ USB Gateway

E5810A LAN/GPIB Gateway

E8491B VXI IEEE 1394 Slot 0(FireWire)5

RS-232

Keysight IO Libraries Suite 2023:

New Feature(s):

  • Added a KDI component as part of IOLS installation
  • Enhanced authentication mechanism:
    • Added SCRAM authentication mechanism for HiSLIP secure connection
    • Enhanced authentication mechanism that assimilates secure configuration data from SIC Expert
  • Enhanced VISA Interfaces with the implementation of the VISA specification v7.2
    • Added new PXI attributes for VISA-C, VISA.NET and VISA-COM
    • Added secure connection support for VISA-C, VISA.NET, and VISA-COM
  • Enhanced Connection Expert user interface:
    • The newly improved Lan instrument Add/Edit screen
      • allows the addition of multiple HiSLIP addresses and
      • shows the connection status of an instrument (a green lock indicates a secure connection whereas a grey lock indicates the connection is not secure)
    • Added HTTPS support for the instrument web page.
    • The newly improved ASRL Options screen provides toggle options for enabling or disabling ASRL sticky behavior and auto-discovery.
  • VISA Shared Component version 7.2
  • Windows on ARM does not support Serial Interface or Serial Instrument.
Note: VXI is not supported on Windows 8 and Windows 11

Known Issues

  • You may need to install .NET Framework 3.5 for 32-bit VISA applications.
  • You can install .NET Framework 3.5 using the IO Libraries Suite installer with the net35 directive. For example: IOLibSuite_version.exe /s /z"typical;net35"
IO Libraries Suite 2022 Update 2(for Windows)

Windows 10 Windows 8.1 Windows 7 SP1 Windows Server 2012 & 2016 (64-bit only) Windows Server 2008 R2 SP1 (64-bit only)

USB instruments

LAN instruments 3

PXI Interface4

82350B/C PCI GPIB Interface

82351A/B PCIe® GPIB Interface

82357A/B USB/GPIB Interface

E1406A VXI Command Module (GPIB)5

E5810B LAN/GPIB/ USB Gateway

E5810A LAN/GPIB Gateway

E8491B VXI IEEE 1394 Slot 0(FireWire)5

RS-232

Keysight IO Libraries Suite 2022 Update 2:

New Feature(s): None

Note: Removed support for Data Analytics.

Known Issues:

  • You may need to install .NET Framework 3.5 for 32-bit VISA applications to work.
    You can install .NET Framework 3.5 using the IO Libraries Suite installer with the net35 directive. For example: IOLibSuite_version.exe /s /z"typical;net35"

IO Libraries Suite 2022(for Windows on ARM) Windows 10 on ARM (32-bit x86 emulated applications): Home Pro Enterprise

USB instruments

LAN instruments 3

82357A/B USB/GPIB Interface

E5810B LAN/GPIB/ USB Gateway

E5810A LAN/GPIB Gateway

RS-232

IO Libraries Suite 2022 adds support for ARM based Windows systems.

Major features supported:

  • Utilities including Connection Expert, the Instrument Discovery Service, Interactive IO, and IO Monitor.
  • IO Interface supported: LAN (HiSLIP, VXI-11/SICL-LAN, and SOCKET), USB/GPIB, USBTMC, RS-232, Remote GPIB, and Remote USB
  • Programming libraries for VISA and SICL

Major features NOT supported:

  • PXI/AXIe
  • VXI
  • Remote IO Server
  • Side-by-Side installation with another vendor's VISA implementation.
  • Programming libraries for VISA.NET and VISA COM
  • Keysight 488

IO Libraries Suite 2022(for Windows)

Windows 10 Windows 8.1 Windows 7 SP1 Windows Server 2012 & 2016 (64-bit only) Windows Server 2008 R2 SP1 (64-bit only)

 

USB instruments

LAN instruments 3

PXI Interface4

82350B/C PCI GPIB Interface

82351A/B PCIe® GPIB Interface

82357A/B USB/GPIB Interface

E1406A VXI Command Module (GPIB)5

E5810B LAN/GPIB/ USB Gateway

E5810A LAN/GPIB Gateway

E8491B VXI IEEE 1394 Slot 0(FireWire)5

RS-232

Keysight IO Libraries Suite 2022:

New Feature(s):

  • Upgraded VISA Shared Component to 7.1.1.

Defect fixes:

  • Fixed some miscellaneous defects, including VISA-COM backward compatibility issue.

Known Issues:

  • You must install the VNA software before connecting the USB products, or else the chassis may appear under the PXI10 interface in Connection Expert.
    To fix this issue, install the VNA software, disconnect the chassis, and re-connect them.

  • You may need to install .NET Framework 3.5 for 32-bit VISA applications to work. You can install .NET Framework 3.5 using the IO Libraries Suite installer with the net35 directive. For example: IOLibSuite_version.exe /s /z"typical;net35"

IO Libraries Suite 2021 Update 1(for Windows)

Windows 10 Windows 8.1 Windows 7 SP1 Windows Server 2012 & 2016 (64-bit only) Windows Server 2008 R2 SP1 (64-bit only)

 

USB instruments

LAN instruments 3

PXI Interface4

82350B/C PCI GPIB Interface

82351A/B PCIe® GPIB Interface

82357A/B USB/GPIB Interface

E1406A VXI Command Module (GPIB)5

E5810B LAN/GPIB/ USB Gateway

E5810A LAN/GPIB Gateway

E8491B VXI IEEE 1394 Slot 0(FireWire)5

RS-232

Keysight IO Libraries Suite 2021 adds support for secure instrument communication:
  • Added support for Thunderbolt Port connection with P6005B/P6006B Streamline Series VNA products.

    Refer to the P600XB & P50XXB release notes for supported PCs.

Defect fixes:

  • Fixed some issues related to the PXI system (while it's connected).

Known Issues:

  • A backward compatibility issue with VISA Shared Components 7.1 and Keysight Instrument or Measurement software using the instrument’s IVI-COM drivers. If you have this setup, do not update to IOLS 2021 Update 1. IOLS 2020 U1 has VISA Shared Components 5.12 without this issue.
    We are currently working with IVI.org and other test and measurement vendors to resolve this issue.
  • You must install the VNA software before connecting the P6005A/P6006A chassis, or else the chassis may appear under the PXI10 interface in Connection Expert.
    To fix this issue, install the VNA software, disconnect the chassis, and re-connect them.
  • You may need to install .NET Framework 3.5 for 32-bit VISA applications to work. You can install .NET Framework 3.5 using the IO Libraries Suite installer with the net35 directive. For example: IOLibSuite_version.exe /s /z"typical;net35"
IO Libraries Suite 2021 (for Linux) Red Hat 7.4 -8.3, CentOS 7.4- 8.3 (except 8.1 and 8.2), Ubuntu 18.04.x, 20.04, 20.04.1, and 20.04.2 LAN (HiSLIP, VXI-11/SICL-LAN, and SOCKET), PCI/PCIe GPIB, USB/GPIB, USBTMC, RS-232, Remote GPIB, Remote USB, and Remote RS-232

IO Libraries Suite 2021 (for Linux) includes the following new features:

  • Extends support to select versions of Ubuntu, CentOS, and RedHat.

  • Adds DKMS technology, which potentially enables use on additional distributions and versions. (Although DKMS enables the use of versions other than those listed below, those other versions are not supported by Keysight.)

  • Incorporates the IVI standard USBTMC kernel driver, which improves multi-vendor interoperability.

IO Libraries Suite 2021 (for Windows) Windows 10 Windows 8.1 Windows 7 SP1 Windows Server 2012 & 2016 (64-bit only) Windows Server 2008 R2 SP1 (64-bit only)

USB instruments

LAN instruments 3

PXI Interface4

82350B/C PCI GPIB Interface

82351A/B PCIe® GPIB Interface

82357A/B USB/GPIB Interface

E1406A VXI Command Module (GPIB)5

E5810B LAN/GPIB/ USB Gateway

E5810A LAN/GPIB Gateway

E8491B VXI IEEE 1394 Slot 0(FireWire)5

RS-232

IO Libraries Suite 2021 (for Windows) adds support for secure instrument communication:

  • Support HiSLIP (IVI-6.1) Revision 2.0

  • Support VISA (VPP-4.3) Revision 7.1

  • VISA Shared Components - Upgrade to 7.1

Defect fixes:

  • A PXIe module interoperability issue is fixed. With this fix, Keysight VISA can properly handle other vendor's PXIe modules when Keysight PXI Resource Manager is not the active one.

  • An interrupt handling issue with HiSLIP devices is fixed.

IO Libraries Suite 2020 Update 1 (for Windows)

Windows 10 Windows 8.1 Windows 7 SP1 Windows Server 2012 & 2016 (64-bit only) Windows Server 2008 R2 SP1 (64-bit only)

USB instruments

LAN instruments 3

PXI Interface4

82350B/C PCI GPIB Interface

82351A/B PCIe® GPIB Interface

82357A/B USB/GPIB Interface

E1406A VXI Command Module (GPIB)5

E5810B LAN/GPIB/ USB Gateway

E5810A LAN/GPIB Gateway

E8491B VXI IEEE 1394 Slot 0(FireWire)5

RS-232

IO Libraries Suite 2020 Update 1 (for Windows) fixed the following issues:

  • The discovery process issue for the 1394-VXI interface when the VXI system is using MXI connections.
  • The memory leaking issues in the Keysight Instrument Discovery Service and LxiMdnsBrowser.

 

IO Libraries Suite 2020 (for Windows)

Windows 10 Windows 8.1 Windows 7 SP1 Windows Server 2012 & 2016 (64-bit only) Windows Server 2008 R2 SP1 (64-bit only)

USB instruments

LAN instruments 3

PXI Interface4

82350B/C PCI GPIB Interface

82351A/B PCIe® GPIB Interface

82357A/B USB/GPIB Interface

E1406A VXI Command Module (GPIB)5

E5810B LAN/GPIB/ USB Gateway

E5810A LAN/GPIB Gateway

E8491B VXI IEEE 1394 Slot 0(FireWire)5

RS-232

IO Libraries Suite 2020 provided several enhancements:

  • General performance enhancements.
  • VISA Shared Components - Upgrade to 5.12.
  • Support for GPIB drivers with Windows 10 Device Guard.
  • Bug fixes and minor enhancements including: When NI is the primary resource manager, Connection Expert now reports all NI PXI modules. On systems with NI VISA, an install repair operation completes fully. When the NI PXI system module is used with Keysight Resource Manager as the primary resource manager, the full address of the system module is now reported correctly. Serial instrument detection is fixed. Following an upgrade, the GPIB instrument list is properly refreshed. Checking status on a LAN instrument completes without interrupting instrument discovery. Serial ports, which were not displaying in Connection Expert in certain configurations, are now visible.

IO Libraries Suite 2020 (for Linux) 

CentOS 7.1 - 7.6

Red Hat 7.1 - 7.6

Ubuntu 16.04.x and 18.04.x (to be updated in the next release)

LAN (HiSLIP, VXI-11/SICL-LAN, and SOCKET), PCI/PCIe GPIB, USB/GPIB, USBTMC, RS-232, Remote GPIB, Remote USB, and Remote RS-232 IO Libraries Suite 2020 extended support to select versions of Ubuntu. Other revisions were minor.

IO Libraries Suite 2019 Update 1 (for Windows)

Windows 10 (32/64-bit): Windows 10 Home, Windows 10 Pro, Windows 10 Enterprise

Windows 8 and 8.1 (32/64-bit): Windows 8/8.1, Windows 8/8.1 Pro, Windows 8/8.1 Enterprise

Windows 7 SP1 (32/64-bit): Starter, Home Basic, Home Premium, Professional, Ultimate, Enterprise

Windows Server 2008 R2 SP1 (64-bit): Standard and Enterprise

Windows Server 2012 (64-bit): Standard

Windows Server 2016 (64-bit): Standard

USB instruments

LAN instruments 3

PXI Interface4

82350B/C PCI GPIB Interface

82351A/B PCIe® GPIB Interface

82357A/B USB/GPIB Interface

E1406A VXI Command Module (GPIB)5

E5810B LAN/GPIB/ USB Gateway

E5810A LAN/GPIB Gateway

E8491B VXI IEEE 1394 Slot 0(FireWire)5

RS-232

  • Enhanced USB-PXI discovery to better handle slow module initialization.

  • Enhanced AXIe chassis support.

  • Added back SICL library support of Visual Basic 6.

  • Fixed a PXIe interoperability issue.

  • Fixed an issue with Keysight Connection Expert reporting of floating PXI modules.

IO Libraries Suite 2019 Update 1 (for Linux)

CentOS 7.1 - 7.6

Red Hat 7.1 - 7.6

USB instruments 1

LAN instruments 3

82350B/C PCI GPIB Interface

82351A/B PCIe® GPIB Interface

82357A/B USB/GPIB Interface

E5810B LAN/GPIB/ USB Gateway

E5810A LAN/GPIB Gateway

RS-232

First update to the original Linux release. Revisions/enhancements as follows: 

  • Support for CentOS and Red Hat 7.6.
  • Minor revisions and bug fixes.
  • A defect was fixed enabling large buffers to be received over USB .

IO Libraries Suite 2019 (for Windows)

Windows 10 (32/64-bit): Windows 10 Home, Windows 10 Pro, Windows 10 Enterprise

Windows 8 and 8.1 (32/64-bit): Windows 8/8.1, Windows 8/8.1 Pro, Windows 8/8.1 Enterprise

Windows 7 SP1 (32/64-bit): Starter, Home Basic, Home Premium, Professional, Ultimate, Enterprise

Windows Server 2008 R2 SP1 (64-bit): Standard and Enterprise

Windows Server 2012 (64-bit): Standard

Windows Server 2016 (64-bit): Standard

USB instruments

LAN instruments 3

PXI Interface4

82350B/C PCI GPIB Interface

82351A/B PCIe® GPIB Interface

82357A/B USB/GPIB Interface

E1406A VXI Command Module (GPIB)5

E5810B LAN/GPIB/ USB Gateway

E5810A LAN/GPIB Gateway

E8491B VXI IEEE 1394 Slot 0(FireWire)5

RS-232

  • Enhanced discovery capabilities:
    • Software servers: IO Libraries Suite can now discover measurement software that has SCPI servers, without any user interaction. Discovered software servers will be displayed in Connection Expert - Instrument View.
    • Hardware servers: IO Libraries Suite now discovers SCPI servers for modular (PXIe/AXIe) instruments that support SCPI communication, providing an additional VISA address in the modular instrument details.
  • Connection Expert now displays additional details for PXIe instruments that have multi-slot, multi-link or multi-endpoint configurations.
  • Shared components – VISA and VISA.NET shared components have been upgraded to 5.11.
  • Support for Windows Server 2016.

IO Libraries Suite 2019 (for Linux)

CentOS 7.1, 7.2, 7.3, 7.4, 7.5

Red Hat 7.1, 7.2, 7.3, 7.4, 7.5

USB instruments 1

LAN instruments 3

82350B/C PCI GPIB Interface

82351A/B PCIe® GPIB Interface

82357A/B USB/GPIB Interface

E5810B LAN/GPIB/ USB Gateway

E5810A LAN/GPIB Gateway

RS-232

First release

IO Libraries Suite 2018

Update 1.0


Windows 10 (32/64-bit): Windows 10 Home, Windows 10 Pro, Windows 10 Enterprise

Windows 8 and 8.1 (32/64-bit): Windows 8/8.1, Windows 8/8.1 Pro, Windows 8/8.1 Enterprise

Windows 7 SP1 (32/64-bit): Starter, Home Basic, Home Premium, Professional, Ultimate, Enterprise

Windows Server 2008 R2 SP1 (64-bit): Standard and Enterprise

Windows Server 2012 (64-bit): Standard

USB instruments

LAN instruments 3

PXI Interface4

82350B/C PCI GPIB Interface

82351A/B PCIe® GPIB Interface

82357A/B USB/GPIB Interface

E1406A VXI Command Module (GPIB)5

E5810B LAN/GPIB/ USB Gateway

E5810A LAN/GPIB Gateway

E8491B VXI IEEE 1394 Slot 0(FireWire)5

RS-232

Keysight IO Libraries Suite 2018 Update 1.0 provides several enhancements:

  • Support for Keysight Streamline Series USB Vector Network Analyzer
  • Support for E1406A GPIB to VXI on Windows 7 and Windows 10
  • Includes the following IVI Foundation shared components:
    • VISA Shared Components 5.10
    • IVI Shared Components 2.5
    • IVI.NET Shared Components 1.4

IO Libraries Suite 2018

Update 0.2


Windows 10 (32/64-bit): Windows 10 Home, Windows 10 Pro, Windows 10 Enterprise

Windows 8 and 8.1 (32/64-bit): Windows 8/8.1, Windows 8/8.1 Pro, Windows 8/8.1 Enterprise

Windows 7 SP1 (32/64-bit): Starter, Home Basic, Home Premium, Professional, Ultimate, Enterprise

Windows Server 2008 R2 SP1 (64-bit): Standard and Enterprise

Windows Server 2012 (64-bit): Standard

USB instruments

LAN instruments 3

PXI Interface4

82350B/C PCI GPIB Interface

82351A/B PCIe® GPIB Interface

82357A/B USB/GPIB Interface

E5810B LAN/GPIB/ USB Gateway

E5810A LAN/GPIB Gateway

E8491B VXI IEEE 1394 Slot 0(FireWire)5

RS-232

Keysight IO Libraries Suite 2018 Update 0.2 fixes the following defects:

  • IO Libraries Suite installer would hang if other applications were doing I/O
  • Some Keysight PXIe cards were not enumerated correctly
  • Keysight VISA was unable to report all PXI devices with viFindRsrc
  • The Connection Expert Chassis tab showed incorrect addresses for some PXI modules
  • Connection Expert was unable to set LU values of 14, 15, 17, or 18 on Keysight USB/GPIB adapters
  • Keysight VISA connections failed when using the VXI-11.2 protocol

IO Libraries Suite 2018

Update 0.1


Windows 10 (32/64-bit): Windows 10 Home, Windows 10 Pro, Windows 10 Enterprise

Windows 8 and 8.1 (32/64-bit): Windows 8/8.1, Windows 8/8.1 Pro, Windows 8/8.1 Enterprise

Windows 7 SP1 (32/64-bit): Starter, Home Basic, Home Premium, Professional, Ultimate, Enterprise

Windows Server 2008 R2 SP1 (64-bit): Standard and Enterprise

Windows Server 2012 (64-bit): Standard

USB instruments

LAN instruments 3

PXI Interface4

82350B/C PCI GPIB Interface

82351A/B PCIe® GPIB Interface

82357A/B USB/GPIB Interface

E5810B LAN/GPIB/ USB Gateway

E5810A LAN/GPIB Gateway

E8491B VXI IEEE 1394 Slot 0(FireWire)5

RS-232

Keysight IO Libraries Suite 2018 Update 0.1 fixed the following issues:

  • Issues that caused Connection Expert to:
    • Get stuck on the Loading Instruments… screen
    • Load images very slowly if internet access was unavailable
  • Automatic scanning for PXI devices after initial boot has been disabled to fix a defect where PXI configuration could get lost on large systems

IO Libraries Suite 2018



Windows 10 (32/64-bit): Windows 10 Home, Windows 10 Pro, Windows 10 Enterprise

Windows 8 and 8.1 (32/64-bit): Windows 8/8.1, Windows 8/8.1 Pro, Windows 8/8.1 Enterprise

Windows 7 SP1 (32/64-bit): Starter, Home Basic, Home Premium, Professional, Ultimate, Enterprise

Windows Server 2008 R2 SP1 (64-bit): Standard and Enterprise

Windows Server 2012 (64-bit): Standard

USB instruments

LAN instruments 3

PXI Interface4

82350B/C PCI GPIB Interface

82351A/B PCIe® GPIB Interface

82357A/B USB/GPIB Interface

E5810B LAN/GPIB/ USB Gateway

E5810A LAN/GPIB Gateway

E8491B VXI IEEE 1394 Slot 0(FireWire)5

RS-232

Note: Windows version 8.1 and Windows Server version 2012 R2 require Windows update 2919355 before Keysight IO Libraries can be properly installed.

Added Support:

  • E8491B support forWindows 10
  • Keysight USB/PXI devices

IO Libraries Suite 2017 Update 1

Windows 10 (32/64-bit): Windows 10 Home, Windows 10 Pro, Windows 10 Enterprise

Windows 8 and 8.1 (32/64-bit): Windows 8/8.1, Windows 8/8.1 Pro, Windows 8/8.1 Enterprise

Windows 7 SP1 (32/64-bit): Starter, Home Basic, Home Premium, Professional, Ultimate, Enterprise

Windows Server 2008 R2 SP1 (64-bit): Standard and Enterprise

Windows Server 2012 (64-bit): Standard

USB instruments

LAN instruments 3

PXI Interface4

82350B/C PCI GPIB Interface

82351A/B PCIe® GPIB Interface

82357A/B USB/GPIB Interface

E5810B LAN/GPIB/ USB Gateway

E5810A LAN/GPIB Gateway

E8491B VXI IEEE 1394 Slot 0 (FireWire)5

RS-232

Note: Windows version 8.1 and Windows Server version 2012 R2 require Windows update 2919355 before Keysight IO Libraries can be properly installed.

IO Libraries Suite 2017

Windows 10 (32/64-bit): Windows 10 Home, Windows 10 Pro, Windows 10 Enterprise

Windows 8 and 8.1 (32/64-bit): Windows 8/8.1, Windows 8/8.1 Pro, Windows 8/8.1 Enterprise

Windows 7 SP1 (32/64-bit): Starter, Home Basic, Home Premium, Professional, Ultimate, Enterprise

Windows Server 2008 R2 SP1 (64-bit): Standard and Enterprise

Windows Server 2012 (64-bit): Standard

USB instruments

LAN instruments 3

PXI Interface4

82350B/C PCI GPIB Interface

82351A/B PCIe® GPIB Interface

82357A/B USB/GPIB Interface

E5810B LAN/GPIB/ USB Gateway

E5810A LAN/GPIB Gateway

E8491B VXI IEEE 1394 Slot 0 (FireWire)5

RS-232

Note: Windows version 8.1 and Windows Server version 2012 R2 require Windows update 2919355 before Keysight IO Libraries can be properly installed.

Added Support:

  • PXI Multi-Module Instruments

IO Libraries Suite 17.3


Windows 10 (32-bit and 64-bit)
Home, Pro, Enterprise, Education

Windows 8 and 8.1 (32-bit and 64-bit)
Windows 8/8.1, Windows 8/8.1 Pro, Windows 8/8.1 Enterprise

Windows 7 SP1 (32-bit and 64-bit)

Starter, Home Basic, Home Premium, Professional, Ultimate, Enterprise

Windows Server 2008 R2 SP1
(64-bit), Standard and Enterprise

Windows Server 2012 (64-bit)
Standard

USB instruments

LAN instruments 3

PXI Interface4

82350C PCI GPIB Interface

82351B PCIe® GPIB Interface

82350B 5V PCI GPIB Interface

82351A PCIe® GPIB Interface

82357A/B USB/GPIB Interface

E5810B LAN/GPIB/ USB Gateway

E5810A LAN/GPIB Gateway  

E8491B VXI IEEE 1394 Slot 0
(FireWire)5

RS-232

 

IO Libraries Suite 17.2


Windows 10 (32-bit and 64-bit)
Home, Pro, Enterprise, Education

Windows 8 and 8.1 (32-bit and 64-bit)
Windows 8/8.1, Windows 8/8.1 Pro, Windows 8/8.1 Enterprise

Windows 7 SP1 (32-bit and 64-bit)

Starter, Home Basic, Home Premium, Professional, Ultimate, Enterprise

Windows Server 2008 R2 SP1
(64-bit), Standard and Enterprise

Windows Server 2012 (64-bit)
Standard

USB instruments

LAN instruments 3

PXI Interface4

82350C PCI GPIB Interface

82351B PCIe® GPIB Interface

82350B 5V PCI GPIB Interface

82351A PCIe® GPIB Interface

82357A/B USB/GPIB Interface

E5810B LAN/GPIB/ USB Gateway

E5810A LAN/GPIB Gateway  

E8491B VXI IEEE 1394 Slot 0
(FireWire)5

RS-232

Added Support:

  • Windows 10
  • VISA.NET

No Longer Supports:

  • Windows XP
  • Windows Vista

IO Libraries Suite 17.1


Windows 8 and 8.1 (32-bit and 64-bit)
Windows 8/8.1, Windows 8/8.1 Pro, Windows 8/8.1 Enterprise

Windows 7 SP1 (32-bit and 64-bit)

Starter, Home Basic, Home Premium, Professional, Ultimate, Enterprise

Windows XP SP3
(32-bit versions only) Professional and Home

Windows Vista SP1 and SP2
(32-bit and 64-bit), Business, Ultimate, Enterprise, Home Basic, and Home Premium 

Windows Server 2008 R2 SP1
(64-bit), Standard and Enterprise

Windows Server 2012 (64-bit)
Standard

USB instruments

LAN instruments 3

PXI Interface4

82350C PCI GPIB Interface

82351B PCIe® GPIB Interface

82350B 5V PCI GPIB Interface

82351A PCIe® GPIB Interface

82357A/B USB/GPIB Interface

E5810B LAN/GPIB/ USB Gateway

E5810A LAN/GPIB Gateway  

E8491B VXI IEEE 1394 Slot 0
(FireWire)5

RS-232

IO Libraries Suite 17.1 can be installed in instruments.

Added Support:

  • 82350C PCI GPIB Interface
  • 82351B PCIe® GPIB Interface

No Longer Supports:

  • E1406A VXI Command Module (GPIB)
  • VXI is NOT supported on Windows 8.1, Windows 8, or Windows Server 2012.

IO Libraries Suite 17.0

Windows 8 and 8.1 (32-bit and 64-bit)
Windows 8/8.1, Windows 8/8.1 Pro, Windows 8/8.1 Enterprise

Windows 7 SP1 (32-bit and 64-bit)

Starter, Home Basic, Home Premium, Professional, Ultimate, Enterprise

Windows XP SP3
(32-bit versions only) Professional and Home

Windows Vista SP1 and SP2
(32-bit and 64-bit), Business, Ultimate, Enterprise, Home Basic, and Home Premium 

Windows Server 2008 R2 SP1
(64-bit), Standard and Enterprise

Windows Server 2012 (64-bit)
Standard

USB instruments

LAN instruments 3

PXI Interface4

82350B 5V PCI GPIB Interface

82351A PCIe® GPIB Interface

82357A/B USB/GPIB Interface

E5810B LAN/GPIB/ USB Gateway

E5810A LAN/GPIB Gateway  

E8491B VXI IEEE 1394 Slot 0
(FireWire)5

RS-232

Now the Keysight IO Libraries Suite.

Added Support:

  • Windows 8.1
  • E5810B LAN/GPIB/ USB Gateway

No Longer Supports:

  • E1406A VXI Command Module (GPIB)
  • VXI is NOT supported on Windows 8.1, Windows 8, or Windows Server 2012.

New Connection Expert

New Add Legacy PXI Chassis Utility

IO Libraries Suite 16.3

Windows XP SP3
(32-bit versions only) Professional and Home

Windows Vista SP1 and SP2
(32-bit and 64-bit), Business, Ultimate, Enterprise, Home Basic, and Home Premium 

Windows 7 SP1 (32-bit and 64-bit)
Starter, Home Basic, Home Premium, Professional, Ultimate, Enterprise

Windows 8 (32-bit and 64-bit)
Windows 8, Windows 8 Pro, Windows 8 Enterprise

Windows Server 2008 R2 SP1
(64-bit), Standard and Enterprise

Windows Server 2012 (64-bit)
Standard

USB instruments
LAN instruments 3

PXI Interface4

82350B 5V PCI GPIB Interface

82351A PCIe® GPIB Interface

82357A/B USB/GPIB Interface

E5810A LAN/GPIB Gateway  

E8491B VXI IEEE 1394 Slot 0
(FireWire)5

E1406A VXI Command Module (GPIB)5

RS-232

Added Support:

  • Windows 8
  • Windows Server 2012

  • Support for USB3.0-based USBTMC.

  • Support for composite USBTMC devices. A typical composite USBTMC device contains a USBTMC interface for instrument communications and a USB Mass Storage interface. The mass storage interface allows users to access data on their instrument using Windows Explorer, for example.

No Longer Supports:

  • VXI is NOT supported on Windows 8 or Windows Server 2012.

  • The Agilent IO Libraries Suite > Utilities menu selection has been removed from the Start menu for all operating systems. (The Connection Expert menu selection is still available in the Start menu for older operating systems, and from the Start screen for Windows 8 and Windows Server 2012. You can also launch Connection Expert and most utilities from the IO Control icon on your Windows task bar.)

IO Libraries Suite 16.2

Windows XP
Professional and Home
(32-bit versions only)
SP 3

Windows Vista
SP1 and SP2
(32-bit and 64-bit), Business, Ultimate, Enterprise, Home Basic, and Home Premium 

Windows 7 (SP1) (32-bit and 64-bit) Starter, Home Basic, Home Premium, Professional, Ultimate, Enterprise

Windows Server 2008 R2
(SP1)
(64-bit), Standard and Enterprise

USB instruments 1
LAN instruments 3

PXI Interface4

82350B 5V PCI GPIB Interface

82351A PCIe® GPIB Interface

82357A/B USB/GPIB Interface

E5810A LAN/GPIB Gateway  

E8491B VXI IEEE 1394 Slot 0
(FireWire)

E1406A VXI Command Module (GPIB)

RS-232

Added Support:

  • IPv6 instrument addressing for HiSLIP and Raw Sockets LAN-based instruments.
  • Increased support for AXIe chassis and module discovery.
  • Command Expert on the installation CD and available in the Connection Expert Tools menu.






 

IO Libraries Suite 16.1

Windows XP
Professional and Home
(32-bit versions only)
SP 3

Windows Vista
SP1 and SP2
(32-bit and 64-bit), Business, Ultimate, Enterprise, Home Basic, and Home Premium 

Windows 7 (SP1) (32-bit and 64-bit) Starter, Home Basic, Home Premium, Professional, Ultimate, Enterprise

Windows Server 2008 R2
(SP1)
(64-bit), Standard and Enterprise

USB instruments 1
LAN instruments 3

PXI Interface4

82350B 5V PCI GPIB Interface

82351A PCIe® GPIB Interface

82357A/B USB/GPIB Interface

E5810A LAN/GPIB Gateway  

E8491B VXI IEEE 1394 Slot 0
(FireWire)

E1406A VXI Command Module (GPIB)

RS-232

Added Support:

  • Windows Server 2008 R2 (SP1)
  • 64-Bit VXI
  • SP1 for Windows 7

No Longer Supports:

  • 82350A PCI GPIB Interface




 

IO Libraries Suite 16.0

Windows XP
Professional and Home
(32-bit versions only)
SP 3

Windows Vista
SP1 and SP2
(32-bit and 64-bit), Business, Ultimate, Enterprise, Home Basic, and Home Premium 

Windows 7 (32-bit and 64-bit) Starter, Home Basic, Home Premium, Professional, Ultimate, Enterprise

USB instruments 1

LAN instruments 3

PXI Interface4

82350A PCI GPIB Interface
(Windows XP only)

82350B 5V PCI GPIB Interface

82351A PCIe® GPIB Interface

82357A/B USB/GPIB Interface

E5810A LAN/GPIB Gateway  

E8491B VXI IEEE 1394 Slot 0
(FireWire) 32-bit support only

E1406A VXI Command Module (GPIB) (32-bit support only)

RS-232

Added Support:

No Longer Supports:


  • Windows XP
    Professional and Home
    SP 2
  • E5813 Networked 5-Port USB Hub

 

IO Libraries Suite 15.5

Windows XP
Professional and Home
(32-bit versions only)
SP2 and SP 3

Windows Vista
SP1 and SP2
(32-bit and 64-bit), Business, Ultimate, Enterprise, Home Basic, and Home Premium 

Windows 7 (32-bit and 64-bit) Starter, Home Basic, Home Premium, Professional, Ultimate, Enterprise

USB instruments 1

LAN instruments 3

82357A/B USB/GPIB Interface

E5813A Networked 5-Port USB Hub 2 (Windows XP only) 

E5805A USB/4-Port RS-232 Interface 2(Windows XP only) 

82351A PCIe® GPIB Interface

82350B 5V PCI GPIB Interface



82350A PCI GPIB Interface

(Windows XP only)

E5810A LAN/GPIB Gateway  

E8491B VXI IEEE 1394 Slot 0

(FireWire) 32-bit support only

E1406A VXI Command Module (GPIB) (32-bit support only)

RS-232

  • Support for 64-bit processors (X64). No support for Itanium64 processors.

  • The following configurations are supported:
    • Native 32-bit apps. running on a 32-bit OS
    • Native 64-bit apps. running on a 64-bit OS
    • 32-bit apps running on a 64-bit OS

  • IO Libraries Suite version numbers 15.2 through 15.4 were skipped.

IO Libraries Suite 15.1

Windows 2000
SP4 and later

Windows XP
SP2 and later
Professional and Home)

Windows Vista
SP1 and later
(32-bit only, Business, Ultimate, Enterprise, Home Basic, and Home Premium) 

USB instruments 1

LAN instruments 3

82357A/B USB/GPIB Interface

E5813A Networked 5-Port USB Hub 2(Windows XP, 2000 only) 

E5805A USB/4-Port RS-232 Interface 2
(Windows XP, 2000 only) 

82351A PCIe GPIB Interface

82350B 5V PCI GPIB Interface



82350A PCI GPIB Interface

(Windows 2000 and XP only)

E5810A LAN/GPIB Gateway  

E8491B VXI IEEE 1394 Slot 0

(FireWire)

E1406A VXI Command Module (GPIB)

RS-232

  • Improved LAN/LXI instrument discovery

  • Support for LXI 1.3 Standard. Also includes support for IEEE 1588-2008 and mDNS.

  • IO Monitor has significant revision

  • Improved USBTMC User Mode Driver

IO Libraries Suite 15.0

Windows 2000
SP4 and later

Windows XP
SP2 and later
(Professional and Home)

Windows Vista
(32-bit only, Business, Ultimate, and Enterprise) 

USB instruments 1

LAN instruments 3

82357A/B USB/GPIB Interface

E5813A Networked 5-Port USB Hub 2(Windows XP, 2000 only) 

E5805A USB/4-Port RS-232 Interface 2
(Windows XP, 2000 only) 

82351A PCIe GPIB Interface

82350B 5V PCI GPIB Interface

82350A PCI GPIB Interface
(Windows 2000 and XP only)

E5810A LAN/GPIB Gateway  

E8491B VXI IEEE 1394 Slot 0
(FireWire)

E1406A VXI Command Module

(GPIB)

RS-232

  • Improved LAN/LXI instrument discovery

  • IEEE 1588 Timing and Event Triggering support for LXI class B instruments

  • IO Monitor added

IO Libraries Suite 14.2

Windows 2000

Windows XP
(Professional and Home)

USB instruments 1

LAN instruments 3

82357A USB/GPIB Interface

E5813A Networked 5-Port USB Hub 2(Windows XP, 2000 only)

E5805A USB/4-Port RS-232 Interface 2

82350B 5V PCI GPIB Interface
82350A PCI GPIB Interface

E5810A LAN/GPIB Gateway

82341C ISA GPIB Interface
(Windows 2000 only)

E1406A VXI Command Module (GPIB)

E8491B VXI IEEE 1394 Slot 0
(FireWire)

RS-232

  • Agilent 488 library is now disabled by default if another vendor's 488 implementation is installed.

IO Libraries Suite 14.1

Windows 2000

Windows XP
(Professional and Home)

USB instruments 1

LAN instruments 3

82357A USB/GPIB Interface

E5813A Networked 5-Port USB Hub 2
(Windows XP, 2000 only)

E5805A USB/4-Port RS-232 Interface 2

82350B 5V PCI GPIB Interface
82350A PCI GPIB Interface

E5810A LAN/GPIB Gateway

82341C ISA GPIB Interface
(Windows 2000 only)

E1406A VXI Command Module (GPIB)

E8491B VXI IEEE 1394 Slot 0
(FireWire)

RS-232

Added Support:

  • Agilent 488 library, providing compatibility with National Instruments NI-488.2

No Longer Supports:

  • Windows 98 SE 
  • Windows Me

IO Libraries Suite 14.0

Windows 98 SE

Windows Me

Windows 2000

Windows XP
(Professional and Home)

USB instruments 1

LAN instruments 3

82357A USB/GPIB Interface

E5813A Networked 5-Port USB Hub 2 (Windows XP, 2000 only)

E5805A USB/4-Port RS-232 Interface 2

82350B 5V PCI GPIB Interface
82350A PCI GPIB Interface

E5810A LAN/GPIB Gateway

82341C ISA GPIB Interface
(Windows 98 SE, NT 4.0, 2000 only)

E1406A VXI Command Module
(GPIB)

E8491B VXI IEEE 1394 Slot 0
(FireWire)

RS-232

Default paths for IO Libraries Suite changed


Added Support:
  • E5813A Networked 5-Port USB Hub **

No Longer Supports:

  • Windows NT 4.0
  • E2050A/B LAN/GPIB Gateway

IO Libraries
M.01.01

Windows 98 SE

Windows Me

Windows NT 4.0

Windows 2000

Windows XP
(Professional and Home)

USB instruments 1

LAN instruments 3

82357A USB/GPIB Interface

E5805A USB/4-Port RS-232 Interface 2(no Windows NT 4.0 support)

82350B 5V PCI GPIB Interface
82350A PCI GPIB Interface

E5810A LAN/GPIB Gateway
E2050A/B LAN/GPIB Gateway

82341C ISA GPIB Interface
(Windows 98 SE, NT 4.0, 2000 only)

E1406A VXI Command Module
(GPIB)

E8491B VXI IEEE 1394 Slot 0
(FireWire)

RS-232

Added Support:

  • USB instruments 1
  • E5805A USB/4-Port RS-232 Interface
  • VISA-COM installed with the IO Libraries

IO Libraries
M.01.00

(Runtime only)

Windows 98 SE

Windows Me

Windows NT 4.0

Windows 2000

Windows XP
(Professional and Home)

USB instruments 1

LAN instruments 3

82357A USB/GPIB Interface

E5805A USB/4-Port RS-232 Interface 2(no Windows NT 4.0)

82350B 5V PCI GPIB Interface
82350A PCI GPIB Interface

E5810A LAN/GPIB Gateway
E2050A/B LAN/GPIB Gateway

82341C ISA GPIB Interface
(Windows 98 SE, NT 4.0, 2000 only)

E1406A VXI Command Module
(GPIB)

E8491B VXI IEEE 1394 Slot 0
(FireWire)

RS-232

Added Support:

  • USB instruments 1
  • E5805A USB/4-Port RS-232 Interface
  • VISA-COM installed with the IO Libraries

IO Libraries
L.02.01

Windows 98 SE

Windows Me

Windows NT 4.0

Windows 2000

Windows XP Professional

LAN instruments 3

82357A USB/GPIB Interface

82350B 5V PCI GPIB Interface
82350A PCI GPIB Interface

E5810A LAN/GPIB Gateway
E2050A/B LAN/GPIB Gateway

82341C ISA GPIB Interface
(Windows 98 SE, NT 4.0, 2000 only)

E1406A VXI Command Module
(GPIB)

E8491B VXI IEEE 1394 Slot 0
(FireWire)

RS-232

Added Support:

  • 82350B 5V PCI GPIB Interface

IO Libraries
L.02.00

Windows 98 SE

Windows Me

Windows NT 4.0

Windows 2000

Windows XP Professional

LAN instruments 3

82357A USB/GPIB Interface

82350A PCI GPIB Interface

E5810A LAN/GPIB Gateway
E2050A/B LAN/GPIB Gateway

82341C ISA GPIB Interface
(Windows 98 SE, NT 4.0, 2000 only)

E1406A VXI Command Module
(GPIB)

E8491B VXI IEEE 1394 Slot 0
(FireWire)

RS-232

Added Support:

  • 82357A patches
  • Basic for Windows 82350A patches
  • Agilent T&M Toolkit for Visual Studio .NET
  • VISA locking over TCPIP

No Longer Supports:

  • Building IO projects with Microsoft Visual  Studio 5 and earlier due to a change in the .lib file format.

IO Libraries
L.01.01

Windows 98 SE

Windows Me

Windows NT 4.0

Windows 2000

Windows XP Professional

LAN instruments 3

82357A USB/GPIB Interface

82350A PCI GPIB Interface

E5810A LAN/GPIB Gateway
E2050A/B LAN/GPIB Gateway

82341C ISA GPIB Interface
(Windows 98 SE, NT 4.0, 2000 only)

E1406A VXI Command Module
(GPIB)

E8491B VXI IEEE 1394 Slot 0
(FireWire)

RS-232

Added Support:

  • E5810A LAN/GPIB Gateway 
  • Windows XP Professional
  • 82357A USB/GPIB Interface

No Longer Supports:

  • Windows 95 
  • E2075A GPIO

IO Libraries
L.01.00

Windows 98 SE

Windows Me

Windows NT 4.0

Windows 2000

Windows XP Professional

LAN instruments 3

82341C ISA GPIB Interface
(Windows 98 SE, NT 4.0, 2000 only)

82350A PCI GPIB Interface

82357A USB/GPIB Interface

E2050A/B LAN/GPIB Gateway

E1406A VXI Command Module
(GPIB)

E8491B VXI IEEE 1394 Slot 0
(FireWire)

RS-232

Added Support:

  • Windows XP Professional
  • 82357A USB/GPIB Interface

No Longer Supports:

  • Windows 95 
  • E2075A GPIO

IO Libraries
K.01.00

Windows 95

Windows 98 / 98 SE

Windows Me

Windows NT 4.0

Windows 2000

LAN instruments 3

82341C ISA GPIB Interface
(no Windows Me support)

82350A PCI GPIB Interface

E2050A/B LAN/GPIB Gateway

E2075A GPIO Interface
(no Windows Me support)

E1406A VXI Command Module
(GPIB)

E8491B VXI IEEE 1394 Slot 0
(FireWire)

RS-232

Added Support:

  • Single or dual processor support for 82350A, E2050A/B and RS-232 on Windows NT/2000
  • VISA 2.2
  • LAN instruments with VISA
  • NI-488.2 interface cards

No Longer Supports:

  • 82341D GPIB

IO Libraries
J.02.00

Windows 95

Windows 98 / 98 SE

Windows Me

Windows NT 4.0

Windows 2000

LAN instruments 3 (SICL only)

82341C ISA GPIB Interface
(no Windows Me support)

82341D ISA GPIB Interface
(Windows  95 only)

82350A PCI GPIB Interface

E2050A/B LAN/GPIB Gateway

E2075A GPIO Interface
(no Windows Me support)

E1406A VXI Command Module
(GPIB)

E8491B VXI IEEE 1394 Slot 0
(FireWire)

RS-232

Added Support:

  • Windows 2000
  • Windows Me (no support for ISA Interfaces)
  • VISA 1.1
  • Tested 1394 Cardbus cards

Changes:

  • Default paths for IO Libraries have changed

IO Libraries
J.01.02

Windows 95

Windows 98 / 98 SE

Windows Me

Windows NT 4.0

Windows 2000

82350A PCI GPIB Interface

LAN instruments 3 (SICL only)

82341C ISA GPIB Interface
(no Windows Me support)

82341D ISA GPIB Interface
(Windows  95 only)

82350A PCI GPIB Interface

E2050A/B LAN/GPIB Gateway

E2075A GPIO Interface
(no Windows Me support)

E1406A VXI Command Module
(GPIB)

E8491B VXI IEEE 1394 Slot 0
(FireWire)

RS-232

Changes:

  • 82341A GPIB card problem fixed
  • Large block transfers on 1394 Cardbus cards that used the NEC 1394 chipset fixed.

IO Libraries
J.01.01

Windows 95

Windows 98 / 98 SE

Windows Me

Windows NT 4.0

Windows 2000

LAN instruments 3 (SICL only)

82341C ISA GPIB Interface
(no Windows Me support)

82341D ISA GPIB Interface
(Windows  95 only)

82350A PCI GPIB Interface

E2050A/B LAN/GPIB Gateway

E2075A GPIO Interface
(no Windows Me support)

E1406A VXI Command Module
(GPIB)

E8491B VXI IEEE 1394 Slot 0
(FireWire)

RS-232

Changes:

  • E8491A problems on Windows 2000 and Windows 98
  • 82341 GPIB configuration problem on Windows 2000 corrected

IO Libraries
J.01.00

Windows 95

Windows 98 / 98 SE

Windows Me

Windows NT 4.0

Windows 2000

LAN instruments 3 (SICL only)

82341C ISA GPIB Interface
(no Windows Me support)

82341D ISA GPIB Interface
(Windows  95 only)

82350A PCI GPIB Interface

E2050A/B LAN/GPIB Gateway

E2075A GPIO Interface
(no Windows Me support)

E1406A VXI Command Module
(GPIB)

E8491B VXI IEEE 1394 Slot 0
(FireWire)

RS-232

Changes:

  • Windows 2000 support for several interfaces
  • Windows 98 support
     for E8491
     IEEE 1394

IO Libraries
H.01.02

or

IO Libraries
H.01.03
(ships with E985x controllers)

Windows 95

Windows 98

Windows NT 4.0

LAN instruments 3 (SICL only)

82341C ISA GPIB Interface

82341D ISA GPIB Interface
(Windows 95 only)

82350A PCI GPIB Interface

E2050A/B LAN/GPIB Gateway

E2075A GPIO Interface

E1406A VXI Command Module
(GPIB)

E8491A/B VXI IEEE 1394 Slot 0
(FireWire)

VXI Embedded Controllers

RS-232

Added Support:

  • Single or dual processor support of E8491A/B

No Longer Supports:

  • Windows 3.1 and NT 3.51
  • 16-bit applications on Windows 95 and 98

IO Libraries
H.01.00


Windows 95

Windows 98

Windows NT 4.0

LAN instruments 3 (SICL only)

82341C ISA GPIB Interface

82341D ISA GPIB Interface
(Windows 95 only)

82350A PCI GPIB Interface

E2050A/B LAN/GPIB Gateway

E2075A GPIO Interface

E1406A VXI Command Module
(GPIB)

E8491A/B VXI IEEE 1394 Slot 0
(FireWire)

VXI Embedded Controllers

RS-232

Added Support:

  • Support for E8491B

No Longer Supports:

  • Windows 3.1 and NT 3.51
  • 16-bit applications on Windows 95 and 98

IO Libraries
G.02.02

Windows 95

Windows 98

Windows NT 3.51

Windows NT 4.0

LAN instruments 3 (SICL only)

82341C ISA GPIB Interface

82341D ISA GPIB Interface
(Windows 95 only)

82350A PCI GPIB Interface

E2050A/B LAN/GPIB Gateway

E2075A GPIO Interface

E1406A VXI Command Module
(GPIB)

E8491A VXI IEEE 1394 Slot 0
(FireWire)

VXI Embedded Controllers

RS-232

Added Support:

  • Windows 98
  • Single or dual processor support of E8491A

 

IO Libraries
G.02.01

 

G.02.00

 

G.01.01

 

G.01.00

Windows 95

LAN instruments 3 (SICL only)

82335B ISA GPIB Interface

82341C ISA GPIB Interface
(GPIB)

E2075A GPIO Interface

E1406A VXI Command Module
(GPIB)

RS-232

 

IO Libraries
F.01.02

 

F.01.01

 

F.01.00

Windows 3.1

Windows 95

LAN instruments 3 (SICL only)

82335B ISA GPIB Interface
(GPIB)

82341C ISA GPIB Interface
(GPIB)

E2075A GPIO Interface

E1406A VXI Command Module
(GPIB)

RS-232

 

1 USB instruments are those that support the USBTMC or USBTMC-USB488 specifications.

2 The E5813A Networked 5-Port USB Hub and E5805A USB/4-Port RS-232 Interface are shipped with driver software that allows them to appear as additional ports on the Windows system. They are not directly supported by the IO Libraries software, but can be used with the indicated IO Libraries Suite revisions.

3 LAN instruments are VXI-11, SICL-LAN, HiSLIP (IO Libraries version 16.0 and later), or raw sockets.

4 The PXI interface is not a physical interface as are the GPIB, LAN, USB and other physical interfaces. The PXI interface is merely a software representation of an interface. Keysight IO Libraries supports two PXI interfaces, PXI0 and PXI10, allowing the combination of all local physical PXI resources under a single interface named PXI0, and USB/PXI resources under the interface named PXI10. All PXI chassis and modules found by the active PXI Resource Manager are automatically grouped under PXI0 interface. USB/PXI resources are only reported by theKeysight PXI Resource Manager.

5 VXI is not supported on Windows 8 and Windows 11.