Command Expert Overview
This section contains information specific to the Windows product.
Keysight Command Expert is a software application that provides fast and easy instrument control in many PC application environments. You can start Command Expert with a link in the Connection Expert Instruments view. If this link is grayed out or does not appear, you need to install Command Expert.
Command Expert is not installed as part of the Keysight IO Libraries; it must be installed separately. You can get the latest version of Command Expert from: www.keysight.com/find/commandexpert.