IEventTrigger::SetAttribute

Description

Use of this method is discouraged. All the non-deprecated standard attributes are accessible via properties on the appropriate COM interfaces.

VB Prototype

SetAttribute(
  attribute As Long,
  attrState As Variant
)

C++ Prototype

HRESULT SetAttribute(
  long attribute,
  VARIANT attrState
);

Parameters

attribute

The attribute type to modify.

attrState

The value of the attribute.

Return Value

Refer to the table of return codes.

See Also

type, CustomEventTypeNumber, TriggerID, GetAttribute, SetAttribute, Close, IEventTrigger Overview