IHislipInstr2::TlsCipherSuite

Description

Returns the TLS cipher suite used by the connection.

VB Prototype

Dim value As String
value = object.TlsCipherSuite

C++ Prototype

HRESULT get_TlsCipherSuite(
  BSTR* TlsCipherSuite
);

Return Value

Refer to the table of return codes.

See Also

Address, Close, ComponentVersion, ControlREN, DeviceName, EncryptionEnabled, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, HostName, Init, IsHislip, LastStatus, LockRsrc, LockState, MaxMessage, OptionString, OverlapEnabled, ProgID, ProtocolVersion, ResourceName, SaslMechanism, ServerCertificate, ServerCertificateExpirationDate, ServerCertificateIsPerpetual, ServerCertificateIssuerName, ServerCertificateSubjectName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, SpecVersion, Timeout, TlsCipherSuite, UnlockRsrc, IHislipInstr2 Overview