IVxi::CommandQuery

Note: Keysight's VISA COM does not support a COM server for VXI. The IVxi-related interfaces are listed in this help file because they are included in the global VISA COM library.

Description

Sendsthe device a miscellaneous command or query and/or retrieves the response to a previous query.  This operation can send a command or query, or receive a response to a query previously sent to the device.  The mode parameter specifies whether to issue a command and/or retrieve a response, and what type or size of command and/or response to use.

VB Prototype

value As Long = CommandQuery(
  mode As VXICommandQuery,
  cmd As Long
)

C++ Prototype

HRESULT CommandQuery(
  VXICommandQuery mode,
  long cmd,
  long* pResponse
);

Parameters

mode

Specifies whether to issue a command and/or retrieve a response.

cmd

The miscellaneous command to send.

pResponse

The response retrieved from the device.

Return Value

Refer to the table of return codes.

See Also

ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, CommanderLA, DestinationAccessPrivilege, DeviceClass, FastDataChannel, FastDataChannelMode, FastDataChannelUsePair, ImmediateServant, LogicalAddress, MainframeLogicalAddress, ManufacturerID, ManufacturerName, MemoryBase, MemorySize, MemorySpace, ModelCode, ModelName, TriggerID, Slot, SourceAccessPrivilege, TriggerSupport, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, AssertTrigger, CommandQuery, IVxi Overview