IVxiBackplane::ComponentVersion
Note: Keysight's VISA COM does not support a COM server for VXI. The IVxi-related interfaces are listed in this help file because they are included in the global VISA COM library.
Description
A numeric version for this component.
VB Prototype
Dim value As Long
value = object.ComponentVersion
C++ Prototype
HRESULT get_ComponentVersion(
long* ComponentVersion
);
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, MainframeLA, TriggerID, TriggerStatus, TriggerSupport, VxiVmeInterruptStatus, VxiVmeSysfailStatus, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, AssertInterruptSignal, AssertTrigger, AssertUtilSignal, MapTrigger, UnmapTrigger, IVxiBackplane Overview