Keysight VISA.NET Help
Blocking Wait Sample

Blocking Wait Sample

This code sample illustrates an asynchronous read operation with a blocking wait.

Blocking Wait Sample Details

After returning from the BeginRead method, the sample code waits one time for the asyncResult.AsyncWaitHandle event to be signaled. If the WaitOne method returns true (which means that the read succeeded or a timeout did not occur), the data that was read is available, and the sample calls EndReadString to complete the operation. Finally, the sample closes the session.

In the sample, variables are kept with the section in which they are first used.

Initialize

To set the stage, the sample opens a session to a GPIB instrument with the alias MyInstr. Then it sends a *IDN? command to the instrument. The instrument will respond with its identification string. Refer to the IO Libraries Suite Help for details on using aliases.

Initialize
Copy Code
IGpibSession session = null;
session = (IGpibSession)GlobalResourceManager.Open("MyInstr",
                                               Ivi.Visa.AccessModes.None,                             
                                               2000);
 
session.RawIO.Write("*IDN?\n");

Start the Asynchronous Read

Next the sample code calls BeginRead. If it returns a null, then the attempt to begin the read did not succeed, and the sample throws an exception. Without a valid IVisaAsyncResult reference, nothing more can be done.

Start the Read
Copy Code
IVisaAsyncResult asyncResult = null;
var buffer = new byte[1000];
var expectedState = new object();
 
asyncResult = session.RawIO.BeginRead(buffer, expectedState);
 
if (asyncResult == null)
{
  throw new NullReferenceException("BeginRead returned a null reference - could not start asynchronous read.");
}

Wait

Now the sample code uses a WaitHandle returned by the BeginRead method to wait once for a completion event to be signaled. WaitOne returns true if the completion event was signaled because the operation completed successfully, and false if it was signaled because a timeout occurred.

Wait
Copy Code
var completed = false;
 
completed = asyncResult.AsyncWaitHandle.WaitOne(1000);
 
if (!completed)
{
  throw new VisaException("Asynchronous read with blocking wait timed out.");
}

End the Asynchronous Read

Next the sample code calls EndRead. Remember that this is necessary for the asynchronous operation to clean up after itself.

End the Read
Copy Code
var response = string.Empty;
object resultState = null;
 
response = session.RawIO.EndReadString(asyncResult);
resultState = asyncResult.AsyncState;

Close the Session

Finally, the sample closes the session.

Close the Session
Copy Code
session.Dispose();
session = null;

Complete Sample

Here is the complete blocking wait code sample:

Polling Sample
Copy Code
using System;
using Ivi.Visa;
using Keysight.Visa;
 
namespace IdnSample
{
  class IdnSample
  {
    static void Main(string[] args)
    {
      IGpibSession session = null;
      session = (IGpibSession)GlobalResourceManager.Open("MyInstr",
                                                         Ivi.Visa.AccessModes.None,
                                                         2000);
 
      session.RawIO.Write("*IDN?\n");
 
      IVisaAsyncResult asyncResult = null;
      var buffer = new byte[1000];
      var expectedState = new object();
 
      asyncResult = session.RawIO.BeginRead(buffer, expectedState);
 
      if (asyncResult == null)
      {
        throw new NullReferenceException("BeginRead returned a null reference.");
      }
 
      var completed = false;
 
      completed = asyncResult.AsyncWaitHandle.WaitOne(1000);
 
      if (!completed)
      {
        Console.WriteLine("Completed: {0}", asyncResult.IsCompleted.ToString());
        throw new ApplicationException ("Asynchronous read with poll timed out.");
      }
 
      var response = string.Empty;
      object resultState = null;
 
      response = session.RawIO.EndReadString(asyncResult);
      resultState = asyncResult.AsyncState;
 
      Console.WriteLine("Completed: {0}", asyncResult.IsCompleted.ToString());
      Console.WriteLine("Response:  {0}", response.TrimEnd(new char[] { '\n' }));
 
      session.Dispose();
      session = null;
 
      Console.WriteLine("Press any key to end...");
      Console.ReadKey();
    }
  }
}

 

 


© Keysight Technologies 2015-2026