Keysight VISA.NET Help
GpibControllerInChargeEventArgs Class Members
Properties 


The following tables list the members exposed by GpibControllerInChargeEventArgs.

Public Constructors
 NameDescription
Public ConstructorGpibControllerInChargeEventArgs ConstructorInitializes a new instance of the GpibControllerInChargeEventArgs class.  
Top
Public Properties
 NameDescription
Public PropertyCustomEventType A value that uniquely identifies an implementation-specific event type. (Inherited from Ivi.Visa.VisaEventArgs)
Public PropertyEventType The VISA.NET standard event type. (Inherited from Ivi.Visa.VisaEventArgs)
Public PropertyIsControllerInCharge True if the controller for the GPIB interface is in charge.  
Top
See Also

Reference

GpibControllerInChargeEventArgs Class
Ivi.Visa Namespace

 

 


© Keysight Technologies 2015-2025